<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックKits for baremetal controllers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Kits-for-baremetal-controllers/m-p/2410210#M24406</link>
    <description>&lt;P&gt;Hi, I wanted to ask if there are any kits out there that come with a chip programmer and some peripherals to test assembly code on real hardware? I know that this can work on an esp, but I like the fact that it's the absolut minimum. Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 01 Sep 2026 19:41:18 GMT</pubDate>
    <dc:creator>bakugo</dc:creator>
    <dc:date>2026-09-01T19:41:18Z</dc:date>
    <item>
      <title>Kits for baremetal controllers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Kits-for-baremetal-controllers/m-p/2410210#M24406</link>
      <description>&lt;P&gt;Hi, I wanted to ask if there are any kits out there that come with a chip programmer and some peripherals to test assembly code on real hardware? I know that this can work on an esp, but I like the fact that it's the absolut minimum. Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2026 19:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Kits-for-baremetal-controllers/m-p/2410210#M24406</guid>
      <dc:creator>bakugo</dc:creator>
      <dc:date>2026-09-01T19:41:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kits for baremetal controllers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Kits-for-baremetal-controllers/m-p/2410662#M24413</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;The S08PT60-EVK, [MC9S08PT60] is a development hardware board that can help you with your application[&lt;A href="https://www.nxp.com/part/S08PT60-EVK" target="_blank"&gt;S08PT60-EVK Product Information&lt;/A&gt;].&lt;/P&gt;
&lt;P&gt;The onboard interfaces include an RGB LED, a 6-axis digital accelerometer and magnetometer, an ambient temperature sensor, two capacitive touch pads, a potentiometer, two user push-buttons, and IRDA transceiver. Also is compatible with the Arduino pin layout for expansions boards.&lt;/P&gt;
&lt;P&gt;You can read more about the features in the main page:&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/S08PT60-EVK" target="_blank"&gt;S08P MCUs Evaluation Kit | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;And there are available boards buying from the distributors. The software tool to use it is &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1" target="_blank"&gt;CodeWarrior for MCUs (Eclipse IDE) v11.1&lt;/A&gt; available for windows 10/11.; in this tool you can test with assembly code.&lt;/P&gt;
&lt;P&gt;Another board option is &lt;A href="https://www.nxp.com/part/S08PB16-EVK" target="_blank"&gt;S08PB16-EVK Product Information | NXP Semiconductors&lt;/A&gt;, using CodeWarrior too, adding the correspondent &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1" target="_blank"&gt;service pack for S08PB&lt;/A&gt; or programming via debugger P&amp;amp;E Multilink FX or P&amp;amp;E Multilink&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2026 16:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Kits-for-baremetal-controllers/m-p/2410662#M24413</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-09-02T16:59:33Z</dc:date>
    </item>
  </channel>
</rss>