<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: mc9s08qg8 compiler</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-compiler/m-p/2404307#M24391</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;I give you a suggestion on your other post if it could help you in repairing the BDM driver to use the device in CodeWarrior&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-drivers/m-p/2403800#M24389" target="_blank"&gt;mc9s08qg8 drivers&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you confirm if you have consulted with Wiztronics about the driver's usage in their boards, do you have any feedback?&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;</description>
    <pubDate>Wed, 12 Aug 2026 16:54:55 GMT</pubDate>
    <dc:creator>luis_maravilla</dc:creator>
    <dc:date>2026-08-12T16:54:55Z</dc:date>
    <item>
      <title>mc9s08qg8 compiler</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-compiler/m-p/2403490#M24387</link>
      <description>&lt;P&gt;proto type: i have a product using this chip. it is not obsolete. i have the code to compile, from 1980. what i want to do, is update the cs v6.3 code on windows 11. i want to update the product from and evaluation unit to a working unit, to be released to manufacturers of sewing equipment. I have three lines of c code to update the product for production.&amp;nbsp; HISTORY: BOBBIN SHOW &amp;lt; 1980. displayed prototype of unit at the show and sold 15 copies for $150 each. I developed specialized gate array chips at International Microciruits INC(IMI) to implement functions. WELL, the unit was a single use. I got a patent and I put the&amp;nbsp; BOBBIN CONTROLLER "BC" away until 1983.&amp;nbsp; Used the mc9s08qg8 chip to up grade the BC to many more functions. living on welfare, i did not have money to further my business. NOW i took the developed unit out of storage, and being 72 i am trying to finish off the last coding to get the latest functions. i am going to try to sell it big before i die. my last move before i die, i can not loose. If u can not help me further, i am going to TI and use their chips. U have me locked out of your devlopment software. So i got maybe 12 years left, and ur chip is the core of the product. If U R not intersested in this product, i will go to TI. I do not have time to play with you business cycles. I figure if the unit takes off, i can sell 20,000 units. It works better than i tought 43 years ago, So am I in or out. I need the BDM drive for my wiztronics. com board interface and cw 11.1 to finish the final unit off. ALSO, i am still on SS. NO money, only a dream. i can not afford $500 fora P&amp;amp;E USB multilink Universal prgrammer. Maybe u would like to "venture capital" the device. u got the whole c code, which i downloaded to u!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!! the ball is in ur court.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Aug 2026 00:19:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-compiler/m-p/2403490#M24387</guid>
      <dc:creator>joepuhich</dc:creator>
      <dc:date>2026-08-11T00:19:02Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s08qg8 compiler</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-compiler/m-p/2404307#M24391</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;I give you a suggestion on your other post if it could help you in repairing the BDM driver to use the device in CodeWarrior&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-drivers/m-p/2403800#M24389" target="_blank"&gt;mc9s08qg8 drivers&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you confirm if you have consulted with Wiztronics about the driver's usage in their boards, do you have any feedback?&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Wed, 12 Aug 2026 16:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08qg8-compiler/m-p/2404307#M24391</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-08-12T16:54:55Z</dc:date>
    </item>
  </channel>
</rss>