<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 MC9S08QG8  CODE WARRIOR</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-CODE-WARRIOR/m-p/2403116#M24383</link>
    <description>&lt;P&gt;WELL, I WILL HAVE TO SAY GOOD BYE, IF THE DERIVATIVE MC9S08QG8 CAN NOT BE SEEN IN CW V6.3 OR CW 11.1. I HAVE WORKED AT GETTING THIS CODE TO WORK FOR 40 DAYS NOW. U SAID IT WAS OK, BUT I CAN NOT FIND ANY CW V6.3 WINDOWS 11 THAT WILL RUN AND DEBUG IN CW 11.1 OR CD 6.3. IF I AM WRONG , PLEASE LET ME KNOW.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 09 Aug 2026 20:01:55 GMT</pubDate>
    <dc:creator>joepuhich</dc:creator>
    <dc:date>2026-08-09T20:01:55Z</dc:date>
    <item>
      <title>MC9S08QG8  CODE WARRIOR</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-CODE-WARRIOR/m-p/2403116#M24383</link>
      <description>&lt;P&gt;WELL, I WILL HAVE TO SAY GOOD BYE, IF THE DERIVATIVE MC9S08QG8 CAN NOT BE SEEN IN CW V6.3 OR CW 11.1. I HAVE WORKED AT GETTING THIS CODE TO WORK FOR 40 DAYS NOW. U SAID IT WAS OK, BUT I CAN NOT FIND ANY CW V6.3 WINDOWS 11 THAT WILL RUN AND DEBUG IN CW 11.1 OR CD 6.3. IF I AM WRONG , PLEASE LET ME KNOW.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Aug 2026 20:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-CODE-WARRIOR/m-p/2403116#M24383</guid>
      <dc:creator>joepuhich</dc:creator>
      <dc:date>2026-08-09T20:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8  CODE WARRIOR</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-CODE-WARRIOR/m-p/2403804#M24390</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The MC9S08QG8 device is available in CodeWarrior v11.1 under the section S08&amp;gt;HCS08Q Family&amp;gt;MC9S08QG8&lt;/P&gt;
&lt;P&gt;I tested with the following setup:&lt;/P&gt;
&lt;P&gt;OS: Windows 11&lt;/P&gt;
&lt;P&gt;CodeWarrior: 11.1&lt;/P&gt;
&lt;P&gt;Device: MC9S08QG8 in board DEMO9S08QG8&lt;/P&gt;
&lt;P&gt;Debug Connection: Via the connection in board &lt;A href="https://www.nxp.com/pages/mc9s08qg8-demonstration-board:DEMO9S08QG8" target="_blank"&gt;DEMO9S08QG8&lt;/A&gt; (USB-to-BDM interface)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="luis_maravilla_1-1786488162478.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394221i967E9141A6F286B0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="luis_maravilla_1-1786488162478.png" alt="luis_maravilla_1-1786488162478.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 11 Aug 2026 22:45:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-CODE-WARRIOR/m-p/2403804#M24390</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-08-11T22:45:47Z</dc:date>
    </item>
  </channel>
</rss>