<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックM&amp;amp;P Multilink</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2401569#M24367</link>
    <description>&lt;P&gt;I have developed approximately 20 projects using S08 processors and CodeWarrior 11.1 &amp;nbsp;with the P&amp;amp;E Multilink Universal FX debugger. I used an Intel-based MAC with Parallels VM running Windows 7. Everything worked Great!&lt;/P&gt;&lt;P&gt;I now have a new MAC , again running Parallels VM and Windows 11. (no choice). CodeWarrior loaded, but with a message about no device driver. It works fine, but the debugger is not recognised. On the old Mac, Windows Device Manager showed an entry "Jungo Connectivity/Windriver", but on the new MAC the device manager only showed an entry "MULTILINK".&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a number of suggested fixes but the proposed files could not be found,&lt;/P&gt;&lt;P&gt;Can someone please offer me a working solution, even if it means using a different debug probe.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 03 Aug 2026 22:19:38 GMT</pubDate>
    <dc:creator>Julian99</dc:creator>
    <dc:date>2026-08-03T22:19:38Z</dc:date>
    <item>
      <title>M&amp;P Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2401569#M24367</link>
      <description>&lt;P&gt;I have developed approximately 20 projects using S08 processors and CodeWarrior 11.1 &amp;nbsp;with the P&amp;amp;E Multilink Universal FX debugger. I used an Intel-based MAC with Parallels VM running Windows 7. Everything worked Great!&lt;/P&gt;&lt;P&gt;I now have a new MAC , again running Parallels VM and Windows 11. (no choice). CodeWarrior loaded, but with a message about no device driver. It works fine, but the debugger is not recognised. On the old Mac, Windows Device Manager showed an entry "Jungo Connectivity/Windriver", but on the new MAC the device manager only showed an entry "MULTILINK".&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a number of suggested fixes but the proposed files could not be found,&lt;/P&gt;&lt;P&gt;Can someone please offer me a working solution, even if it means using a different debug probe.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Aug 2026 22:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2401569#M24367</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-08-03T22:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: M&amp;P Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2401711#M24368</link>
      <description>&lt;P&gt;If you update from Windows 7 to&amp;nbsp;Windows 11, all the related driver may need to reinstall&lt;/P&gt;&lt;P&gt;CodeWarrior®&amp;nbsp;for MCUs (Eclipse IDE) could be a good choice to select&lt;/P&gt;&lt;H4&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-mcus-eclipse-ide-coldfire-56800-e-dsc-qorivva-56xx-rs08-s08-s12z-11-1:CW-MCU10" target="_blank" rel="noopener"&gt;CodeWarrior®&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;for MCUs (Eclipse IDE) - ColdFire®, 56800/E DSC, Qorivva®&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;56xx, RS08/S08, S12Z - 11.1&lt;/A&gt;&lt;/H4&gt;</description>
      <pubDate>Tue, 04 Aug 2026 08:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2401711#M24368</guid>
      <dc:creator>db16122</dc:creator>
      <dc:date>2026-08-04T08:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: M&amp;P Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2402252#M24373</link>
      <description>&lt;P&gt;I hate Windows and I am not updating from W7 to W11 - it is a new machine (Mac M4) and W7 is not compatible so I have no choice.I have been using CodeWarrior for about 25 years. My question was "which drivers do I need for W11 and where can I find them?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just as a point of interest and nothing to do with this topic, AUTODESK products will no longer run on old Intel-based Macs, so Windows 7 - R.I.P.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Aug 2026 20:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2402252#M24373</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-08-05T20:10:44Z</dc:date>
    </item>
    <item>
      <title>Re: M&amp;P Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2402273#M24374</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I would recommend on using the OS windows 11 for using CodeWarrior v11.1 this is the supported option, not virtual machines; as we can't guarantee that the CodeWarrior Tool work with Virtual Machines&lt;/P&gt;
&lt;P&gt;To download the v11.1, Please refer to &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1" target="_blank"&gt;CodeWarrior for MCUs (Eclipse IDE) v11.1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Wed, 05 Aug 2026 21:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2402273#M24374</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-08-05T21:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: M&amp;P Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2402791#M24377</link>
      <description>&lt;P&gt;Sorry about my other post. I replied to the wrong post (one that I should have closed as solved). You will notice that I have been using CW under a VM for "Many years" and although you can't guarantee it, I know that it works. all I need is the Windows device driver for the Multilink. I think it's somewhere on the P&amp;amp;E website, but I can't find it. So far I have CW running with no problems under windows 11, running in the Parallels VM, loaded in OSX Tahoe.&lt;/P&gt;</description>
      <pubDate>Fri, 07 Aug 2026 08:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2402791#M24377</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-08-07T08:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: M&amp;P Multilink</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2403011#M24381</link>
      <description>&lt;P&gt;As an option you could ask them in their support forum if they have it&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/support/index.cfm" target="_blank"&gt;PEmicro Support Home&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Fri, 07 Aug 2026 22:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M-amp-P-Multilink/m-p/2403011#M24381</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-08-07T22:13:32Z</dc:date>
    </item>
  </channel>
</rss>