<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Is there a simple 8 bit microcontroller/assembly language that is nice to work with?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2390183#M24342</link>
    <description>&lt;P&gt;I'm searching for an 8 bit microcontroller where I can look at the actual hex/binary code. I've been learning 8051 assembly in university and I absolutely love seeing and understand every single instruction and value in the memory. But those microcontrollers are antiquated and need a bunch of "hacks" for compatibility. At least that's what it feels like everytime I put my code onto real hardware. So is there a simple 8 bit assembly language with actual chips I can program simple electronics projects with ?&lt;/P&gt;</description>
    <pubDate>Fri, 03 Jul 2026 07:34:50 GMT</pubDate>
    <dc:creator>verdas</dc:creator>
    <dc:date>2026-07-03T07:34:50Z</dc:date>
    <item>
      <title>Is there a simple 8 bit microcontroller/assembly language that is nice to work with?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2390183#M24342</link>
      <description>&lt;P&gt;I'm searching for an 8 bit microcontroller where I can look at the actual hex/binary code. I've been learning 8051 assembly in university and I absolutely love seeing and understand every single instruction and value in the memory. But those microcontrollers are antiquated and need a bunch of "hacks" for compatibility. At least that's what it feels like everytime I put my code onto real hardware. So is there a simple 8 bit assembly language with actual chips I can program simple electronics projects with ?&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jul 2026 07:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2390183#M24342</guid>
      <dc:creator>verdas</dc:creator>
      <dc:date>2026-07-03T07:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2390549#M24343</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;NXP has&amp;nbsp; catalog for &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit-s08-mcus:HCS08" target="_blank"&gt;8 Bit devices&lt;/A&gt;, you could use &lt;A href="https://www.nxp.com/products/S08SG" target="_blank"&gt;S08SG|8-bit Small Package SG MCUs | NXP Semiconductors&lt;/A&gt; devices,&lt;/P&gt;
&lt;P&gt;S08SG family is an entry-level to mid-range device with general features.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;S08SG devices are included in the CodeWarrior Tool.&lt;/P&gt;
&lt;P&gt;The CodeWarrior tool version 11.1, is supported in windows 11, this tool supports different connections [P&amp;amp;E USB Multilink Universal / USB Multilink, P&amp;amp;E Cyclone, Open Source BDM, P&amp;amp;E Full chip simulation]&lt;/P&gt;
&lt;P&gt;You can download the tool from this link: &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1" target="_blank"&gt;CodeWarrior® for MCUs (Eclipse IDE) v11.1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the CW tool when enter debug, there is a section for&amp;nbsp; Disassembly view that shows the loaded program as assembly language instructions mixed with source code for comparison.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jul 2026 18:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2390549#M24343</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-07-03T18:24:12Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a simple 8 bit microcontroller/assembly language that is nice to work with?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2391402#M24344</link>
      <description>&lt;P&gt;Here are some of the 8-bit controllers you can also explore&lt;BR /&gt;&lt;A href="https://www.ibselectronics.com/part/microchip/pic16lf18326-i-sl/2263047/" target="_blank" rel="noopener"&gt;pic16lf18326-i-sl/2263047&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PIC16LF18326-I/SL BY MICROCHIP IS A 14-PIN 8-BIT MICROCONTROLLER WITH 16KB FLASH 1KB RAM 12-BIT ADC 10 PWM CHANNELS I2C SPI UART INTERFACES LOW POWER CONSUMPTION AND OPERATING VOLTAGE OF 2.3V TO 5.5V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A href="https://www.ibselectronics.com/part/microchip/atmega8l-8mu/258363/" target="_self"&gt;atmega8l-8mu/258363&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;ATMEGA8L-8MU by MICROCHIP is an 8-bit AVR microcontroller with 8MHz frequency, 8KB Flash, 32-pin VQFN, I2C, SPI, UART interfaces, operating at 2.7V-5.5V, and -40°C to 85°C temperature range.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jul 2026 04:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-there-a-simple-8-bit-microcontroller-assembly-language-that/m-p/2391402#M24344</guid>
      <dc:creator>IBSelectronics</dc:creator>
      <dc:date>2026-07-07T04:59:08Z</dc:date>
    </item>
  </channel>
</rss>