<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Getting started with 8 bit microcontrollers in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Getting-started-with-8-bit-microcontrollers/m-p/2370157#M24329</link>
    <description>&lt;P&gt;Hey all, I'm just becoming interested with 8 bit microcontrollers. I would like to build a few things with the absolute cheapest parts possible, like some Chinese LoRa modules, some PIC16LF1503-I/P mcu's, at only $1.50 each, I figure I can afford to play around a bit!&lt;/P&gt;&lt;P&gt;I would like to build some wireless devices that can activate a relay, to do things like open a solenoid to water the garden, turn lights etc...&lt;/P&gt;&lt;P&gt;I have zero idea where to start. How do you program these things? Do I need some kind of interface and development environment, like a USB device I can plug these chips into? And write the code too? What kind of code do most of them read, C? How many kb of memory and ram do I need to execute simple tasks like communicating through a LoRa module and turning on some kind of gpio pin to activate a relay?&lt;/P&gt;&lt;P&gt;Ideally I'm looking for the cheapest possible microcontrollers that can communicate over SPI, have atleast a pin or two that can be activated to control relays or camera's or other devices.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Fri, 22 May 2026 09:45:44 GMT</pubDate>
    <dc:creator>mithishan</dc:creator>
    <dc:date>2026-05-22T09:45:44Z</dc:date>
    <item>
      <title>Getting started with 8 bit microcontrollers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Getting-started-with-8-bit-microcontrollers/m-p/2370157#M24329</link>
      <description>&lt;P&gt;Hey all, I'm just becoming interested with 8 bit microcontrollers. I would like to build a few things with the absolute cheapest parts possible, like some Chinese LoRa modules, some PIC16LF1503-I/P mcu's, at only $1.50 each, I figure I can afford to play around a bit!&lt;/P&gt;&lt;P&gt;I would like to build some wireless devices that can activate a relay, to do things like open a solenoid to water the garden, turn lights etc...&lt;/P&gt;&lt;P&gt;I have zero idea where to start. How do you program these things? Do I need some kind of interface and development environment, like a USB device I can plug these chips into? And write the code too? What kind of code do most of them read, C? How many kb of memory and ram do I need to execute simple tasks like communicating through a LoRa module and turning on some kind of gpio pin to activate a relay?&lt;/P&gt;&lt;P&gt;Ideally I'm looking for the cheapest possible microcontrollers that can communicate over SPI, have atleast a pin or two that can be activated to control relays or camera's or other devices.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 09:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Getting-started-with-8-bit-microcontrollers/m-p/2370157#M24329</guid>
      <dc:creator>mithishan</dc:creator>
      <dc:date>2026-05-22T09:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: Getting started with 8 bit microcontrollers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Getting-started-with-8-bit-microcontrollers/m-p/2371458#M24334</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/S08PT?page=1&amp;amp;nrnd=false&amp;amp;query=%7B%22h802%22%3A%7B%22min%22%3A0.97%2C%22max%22%3A1.27%2C%22type%22%3A%22dual_range%22%2C%22name%22%3A%22Budgetary%20Price%22%7D%7D" target="_blank"&gt;S08PT&lt;/A&gt; or &lt;A href="https://www.nxp.com/products/S08PA" target="_blank"&gt;S08PA&lt;/A&gt;, could be a good fit, both are 8-bit microcontrollers, low price option, SPI and different GPIOs, along other features.&lt;/P&gt;
&lt;P&gt;In the Buy/Parametric Section you can compare Packages, #Terminals, Budget, Flash, RAM,&amp;nbsp; etc&lt;/P&gt;
&lt;P&gt;For more characteristics description please refer to &lt;A href="https://www.nxp.com/docs/en/data-sheet/MC9S08PT16.pdf" target="_blank"&gt;MC9S08PT Data Sheet&lt;/A&gt; Table 1 and &lt;A href="https://www.nxp.com/docs/en/data-sheet/MC9S08PA16_Rev.1.pdf" target="_blank"&gt;MC9S08PA16 Series Data&lt;/A&gt; Table 1&lt;/P&gt;
&lt;P&gt;For programming and creating code for S08 devices the recommend path is using &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-MCU-PROED-EX_11-1" target="_blank"&gt;CodeWarrior&amp;nbsp; for MCUs (Eclipse IDE)&lt;/A&gt; v11.1; The language code used is C. This tool support Connection for P&amp;amp;E USB Multilink Universal FX / USB Multilink, P&amp;amp;E Cyclone and Open Source BDM. To take in consideration for when you adapt your board connections according to the chip of your selection.&lt;/P&gt;
&lt;P&gt;Hope this information help you&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Tue, 26 May 2026 18:23:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Getting-started-with-8-bit-microcontrollers/m-p/2371458#M24334</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-05-26T18:23:29Z</dc:date>
    </item>
  </channel>
</rss>