<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MC908QY4CDWER in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4CDWER/m-p/2369102#M24328</link>
    <description>&lt;P&gt;We used the S19 algorithm files originally provided by Motorola to program MC908QY4CDWER, and then, through our own application, we sent serial commands.&lt;BR /&gt;Attachment is part of the schematic we use for programming; we connect serially to X3 through PTA0 and PTA5.&lt;BR /&gt;However, our application seems to connect, but then it reports a programming error.&lt;/P&gt;&lt;P&gt;To troubleshoot the problem, we used a dedicated programmer and software from SUPERPRO for testing: The steps were: erase, check for blanks, program, verify, erase, check for blanks. However, the test results showed that the program could be erased and rewritten normally.&lt;/P&gt;&lt;P&gt;We don't understand where the problem lies. How can we solve it and successfully program with S19?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;我們使用摩托羅拉提供的 S19 演算法檔案對 MC908QY4CDWER 進行編程，然後透過我們自己的應用程式發送串列命令。&lt;/P&gt;&lt;P&gt;附件是我們用於程式設計的部分原理圖；我們透過 PTA0 和 PTA5 串列連接到 X3。&lt;/P&gt;&lt;P&gt;然而，我們的應用程式似乎連接成功，但隨後報告程式設計錯誤。&lt;/P&gt;&lt;P&gt;為了排查問題，我們使用 SUPERPRO 的專用程式設計器和軟體進行測試：步驟為：擦除、檢查空白、編程、驗證、擦除、檢查空白。然而，測試結果表明程式可以正常擦除和重寫。&lt;/P&gt;&lt;P&gt;我們不明白問題出在哪裡。如何才能解決這個問題，並成功地使用 S19 進行程式設計？&lt;/P&gt;&lt;P&gt;非常感謝。&lt;/P&gt;</description>
    <pubDate>Thu, 21 May 2026 03:58:15 GMT</pubDate>
    <dc:creator>GaryChow</dc:creator>
    <dc:date>2026-05-21T03:58:15Z</dc:date>
    <item>
      <title>MC908QY4CDWER</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4CDWER/m-p/2369102#M24328</link>
      <description>&lt;P&gt;We used the S19 algorithm files originally provided by Motorola to program MC908QY4CDWER, and then, through our own application, we sent serial commands.&lt;BR /&gt;Attachment is part of the schematic we use for programming; we connect serially to X3 through PTA0 and PTA5.&lt;BR /&gt;However, our application seems to connect, but then it reports a programming error.&lt;/P&gt;&lt;P&gt;To troubleshoot the problem, we used a dedicated programmer and software from SUPERPRO for testing: The steps were: erase, check for blanks, program, verify, erase, check for blanks. However, the test results showed that the program could be erased and rewritten normally.&lt;/P&gt;&lt;P&gt;We don't understand where the problem lies. How can we solve it and successfully program with S19?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;P&gt;我們使用摩托羅拉提供的 S19 演算法檔案對 MC908QY4CDWER 進行編程，然後透過我們自己的應用程式發送串列命令。&lt;/P&gt;&lt;P&gt;附件是我們用於程式設計的部分原理圖；我們透過 PTA0 和 PTA5 串列連接到 X3。&lt;/P&gt;&lt;P&gt;然而，我們的應用程式似乎連接成功，但隨後報告程式設計錯誤。&lt;/P&gt;&lt;P&gt;為了排查問題，我們使用 SUPERPRO 的專用程式設計器和軟體進行測試：步驟為：擦除、檢查空白、編程、驗證、擦除、檢查空白。然而，測試結果表明程式可以正常擦除和重寫。&lt;/P&gt;&lt;P&gt;我們不明白問題出在哪裡。如何才能解決這個問題，並成功地使用 S19 進行程式設計？&lt;/P&gt;&lt;P&gt;非常感謝。&lt;/P&gt;</description>
      <pubDate>Thu, 21 May 2026 03:58:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4CDWER/m-p/2369102#M24328</guid>
      <dc:creator>GaryChow</dc:creator>
      <dc:date>2026-05-21T03:58:15Z</dc:date>
    </item>
    <item>
      <title>Re: MC908QY4CDWER</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4CDWER/m-p/2370386#M24330</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Could you help us confirm if you are in Monitor mode?&lt;/P&gt;
&lt;P&gt;Monitor module allows debugging and programming of the microcontroller through a single wire interface with a host computer.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/MC68HC908QY4.pdf" target="_blank"&gt;MC68HC908QY4, MC68HC908QY4, MC68HC908QT4, MC68HC908QY2, MC68HC908QT2, MC68HC908QY1, MC68HC908QT1 - Data Sheet&lt;/A&gt; Chapter 15.3 Monitor Module&lt;/P&gt;
&lt;P&gt;Could you help us bring more details about your application programming setup? Is this setup worked before with the S19 algorithm files from Motorola?&lt;/P&gt;
&lt;P&gt;What is it connected to PTA2 and PTA4?&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 23:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4CDWER/m-p/2370386#M24330</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-05-22T23:45:26Z</dc:date>
    </item>
  </channel>
</rss>