<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MC68332 Replacement &amp;amp; 25MHz -&amp;gt;16MHz Compatibility in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68332-Replacement-amp-25MHz-gt-16MHz-Compatibility/m-p/2329442#M24300</link>
    <description>&lt;DIV&gt;&lt;P&gt;We currently use &lt;STRONG&gt;MC68332ACEH25&lt;/STRONG&gt;&lt;STRONG&gt;&amp;nbsp;(25 MHz)&lt;/STRONG&gt; in our design and are looking for replacement options.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1.&lt;/STRONG&gt; Can you recommend a &lt;STRONG&gt;drop‑in 25 MHz MC68332 replacement&lt;/STRONG&gt; that will work &lt;STRONG&gt;without any firmware changes&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2.&lt;/STRONG&gt; If we replace the 25 MHz device with a &lt;STRONG&gt;16 MHz part&lt;/STRONG&gt; such as &lt;STRONG&gt;SPAKMC332AVFC16&lt;/STRONG&gt;, using the same 32.768 kHz external crystal,&lt;BR /&gt;&lt;STRONG&gt;-Will the system still operate correctly?&lt;/STRONG&gt;&lt;BR /&gt;- Or are &lt;STRONG&gt;firmware updates required&lt;/STRONG&gt; (TPU timing, SCI/QSPI baud rates, PIT, watchdog, etc.)?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/DIV&gt;</description>
    <pubDate>Tue, 10 Mar 2026 06:37:42 GMT</pubDate>
    <dc:creator>Dhanraj9</dc:creator>
    <dc:date>2026-03-10T06:37:42Z</dc:date>
    <item>
      <title>MC68332 Replacement &amp; 25MHz -&gt;16MHz Compatibility</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68332-Replacement-amp-25MHz-gt-16MHz-Compatibility/m-p/2329442#M24300</link>
      <description>&lt;DIV&gt;&lt;P&gt;We currently use &lt;STRONG&gt;MC68332ACEH25&lt;/STRONG&gt;&lt;STRONG&gt;&amp;nbsp;(25 MHz)&lt;/STRONG&gt; in our design and are looking for replacement options.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1.&lt;/STRONG&gt; Can you recommend a &lt;STRONG&gt;drop‑in 25 MHz MC68332 replacement&lt;/STRONG&gt; that will work &lt;STRONG&gt;without any firmware changes&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2.&lt;/STRONG&gt; If we replace the 25 MHz device with a &lt;STRONG&gt;16 MHz part&lt;/STRONG&gt; such as &lt;STRONG&gt;SPAKMC332AVFC16&lt;/STRONG&gt;, using the same 32.768 kHz external crystal,&lt;BR /&gt;&lt;STRONG&gt;-Will the system still operate correctly?&lt;/STRONG&gt;&lt;BR /&gt;- Or are &lt;STRONG&gt;firmware updates required&lt;/STRONG&gt; (TPU timing, SCI/QSPI baud rates, PIT, watchdog, etc.)?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 10 Mar 2026 06:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68332-Replacement-amp-25MHz-gt-16MHz-Compatibility/m-p/2329442#M24300</guid>
      <dc:creator>Dhanraj9</dc:creator>
      <dc:date>2026-03-10T06:37:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC68332 Replacement &amp; 25MHz -&gt;16MHz Compatibility</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68332-Replacement-amp-25MHz-gt-16MHz-Compatibility/m-p/2341439#M24304</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260558"&gt;@Dhanraj9&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;MC68332 family is in End-of-life status this also applies for the&amp;nbsp;SPAKMC332AVFC16.&lt;/P&gt;
&lt;P&gt;The firmware between&amp;nbsp;SPAKMC332AVFC16 and MC68332 could be use without issues, only be aware that all the configurations&amp;nbsp;depending on the system clock will require firmware recalibration like the ones you mention (TPU timing, SCI/QSPI baud rates, PIT, watchdog, etc.).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is not a pin-compatible/software compatible option that is listed as active device, the recommendation is to move to a new 32 bit MCU, due to the number of pins of the package you could review the&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/mcx-arm-cortex-m/mcx-a-series-microcontrollers:MCX-A-SERIES" target="_blank"&gt;MCX A Series Microcontrollers&lt;/A&gt;, if you want a more suitable suggestion for a replacement, please let me know more details about your project.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Mar 2026 20:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC68332-Replacement-amp-25MHz-gt-16MHz-Compatibility/m-p/2341439#M24304</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2026-03-27T20:32:51Z</dc:date>
    </item>
  </channel>
</rss>