<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: CodeWarror</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2326629#M24293</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sorry for the inconveniences, the available version of CodeWarrior for 8-bit processors [CodeWarrior v11.1] is not available for Linux only windows.&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
    <pubDate>Wed, 04 Mar 2026 23:37:22 GMT</pubDate>
    <dc:creator>luis_maravilla</dc:creator>
    <dc:date>2026-03-04T23:37:22Z</dc:date>
    <item>
      <title>CodeWarror</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2326392#M24291</link>
      <description>&lt;P&gt;Does anyone know where I can download a copy of CodeWarrior for 8-bit processors that will run under Linux (Ubuntu)? A general enquiry showed that C/W does run under linux, but all of the links&amp;nbsp;are for windows.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 12:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2326392#M24291</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-03-04T12:16:19Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarror</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2326629#M24293</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sorry for the inconveniences, the available version of CodeWarrior for 8-bit processors [CodeWarrior v11.1] is not available for Linux only windows.&lt;/P&gt;
&lt;P&gt;Best Regards, Luis&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 23:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2326629#M24293</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2026-03-04T23:37:22Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarror</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2402780#M24376</link>
      <description>&lt;P&gt;I know that! I have been using CW for "many years", running under Windows 7 which is running under Dropbox which is running under OSX on my Intel-based MAC. All I want is to do the same thing on my new ARM-based MAC. So far I have installed Dropbox and loaded Windows 11. (earlier versions of Windows are not compatible with the new MACs). I have installed CW 11.1 in Windows and it works.&lt;/P&gt;&lt;P&gt;As I said in my original post CW does not recognise the Multilik debug probe because there is no device driver installed. Please refer to my original post for details of what is required&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Aug 2026 08:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CodeWarror/m-p/2402780#M24376</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2026-08-07T08:13:18Z</dc:date>
    </item>
  </channel>
</rss>