<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Can't Use the Internal Ref OSC in STOP Mode (QG8)?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Use-the-Internal-Ref-OSC-in-STOP-Mode-QG8/m-p/130361#M2427</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;In the 9(S)08QG8, I see where I can keep the Internal Reference Oscillator running when in STOP mode. As I read this I was thinking, "good, I can use that for my RTI timebase when in STOP mode". Then I see that the RTI can only use an EXTERNAL clock or the 1KHz internal oscillator (with an accuracy that I cannot find in the datasheet). Why is there an option to keep the Internal Ref Osc running in STOP3 if it cannot be used as the RTI timebase? Furthermore, I can't see that it's used anywhere in STOP mode. Is it to be left running just to keep the engine warm?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My objective is to have an RTI with fairly good accuracy, and no crystal. (And pulling only a few microamps.) Any suggestions would be appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Mar 2006 22:18:16 GMT</pubDate>
    <dc:creator>Wings</dc:creator>
    <dc:date>2006-03-28T22:18:16Z</dc:date>
    <item>
      <title>Can't Use the Internal Ref OSC in STOP Mode (QG8)?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Use-the-Internal-Ref-OSC-in-STOP-Mode-QG8/m-p/130361#M2427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;In the 9(S)08QG8, I see where I can keep the Internal Reference Oscillator running when in STOP mode. As I read this I was thinking, "good, I can use that for my RTI timebase when in STOP mode". Then I see that the RTI can only use an EXTERNAL clock or the 1KHz internal oscillator (with an accuracy that I cannot find in the datasheet). Why is there an option to keep the Internal Ref Osc running in STOP3 if it cannot be used as the RTI timebase? Furthermore, I can't see that it's used anywhere in STOP mode. Is it to be left running just to keep the engine warm?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My objective is to have an RTI with fairly good accuracy, and no crystal. (And pulling only a few microamps.) Any suggestions would be appreciated.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2006 22:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Use-the-Internal-Ref-OSC-in-STOP-Mode-QG8/m-p/130361#M2427</guid>
      <dc:creator>Wings</dc:creator>
      <dc:date>2006-03-28T22:18:16Z</dc:date>
    </item>
  </channel>
</rss>