<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QE16 A/D in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QE16-A-D/m-p/2202899#M24263</link>
    <description>&lt;P&gt;I am using ProcessorExpert to configure the A/D converter on a QE16CFT (Latest version of CodeWarrior). The ADC appears in the components window and I can select it in the Component Inspector. I have configured it for 10-bit single channel continuous conversion (No interrupt) and Port PTA1 as the analog input.&lt;/P&gt;&lt;P&gt;Under the Methods tab all functions are listed, but the Start and Stop methods are not available - they are Greyed out (showing "don't generate code").&lt;/P&gt;&lt;P&gt;What am I doing wrong? It is hardly surprising that I don't get a "Conversion Complete" flag if I can't even start the facility.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Nov 2025 17:32:52 GMT</pubDate>
    <dc:creator>Julian99</dc:creator>
    <dc:date>2025-11-11T17:32:52Z</dc:date>
    <item>
      <title>QE16 A/D</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QE16-A-D/m-p/2202899#M24263</link>
      <description>&lt;P&gt;I am using ProcessorExpert to configure the A/D converter on a QE16CFT (Latest version of CodeWarrior). The ADC appears in the components window and I can select it in the Component Inspector. I have configured it for 10-bit single channel continuous conversion (No interrupt) and Port PTA1 as the analog input.&lt;/P&gt;&lt;P&gt;Under the Methods tab all functions are listed, but the Start and Stop methods are not available - they are Greyed out (showing "don't generate code").&lt;/P&gt;&lt;P&gt;What am I doing wrong? It is hardly surprising that I don't get a "Conversion Complete" flag if I can't even start the facility.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Nov 2025 17:32:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QE16-A-D/m-p/2202899#M24263</guid>
      <dc:creator>Julian99</dc:creator>
      <dc:date>2025-11-11T17:32:52Z</dc:date>
    </item>
    <item>
      <title>Re: QE16 A/D</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QE16-A-D/m-p/2204684#M24264</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245994"&gt;@Julian99&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you share how you are configuring the Method tab for the ADC?&lt;/P&gt;
&lt;P&gt;If you click on don't generate code, you should be able to change it to generate code.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pablo_Ramos_0-1763067529046.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365573iC5382F6C5090E905/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pablo_Ramos_0-1763067529046.png" alt="Pablo_Ramos_0-1763067529046.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pablo_Ramos_0-1763067529046.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Are you able to make this modification?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Pablo&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Nov 2025 21:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QE16-A-D/m-p/2204684#M24264</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-11-13T21:00:47Z</dc:date>
    </item>
  </channel>
</rss>