<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックDimmer with MC68HC908QT4CP</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2157087#M24208</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Following this article&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2839.pdf" target="_blank"&gt;AN2839: Implementing a Lamp Dimmer with an HC908Q Family MCU&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I got&amp;nbsp;MC68HC908QT4CP.&lt;BR /&gt;&lt;BR /&gt;I am looking for programmator and application to support it, I got the code from the nxp article above.&lt;BR /&gt;&lt;BR /&gt;Looking at this forum, I could use CodeWarrior Dev Studio v11 or CodeWarrior Classic 6.3?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;What else I would need to get that code into chip:&amp;nbsp;USBMULTILINK08,&amp;nbsp;M68CPA08P40B56, anything else? I have ALL-07 but don't think it supports it.&lt;BR /&gt;&lt;BR /&gt;Thanks&amp;nbsp;&lt;BR /&gt;hajsenberg&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 24 Aug 2025 19:37:53 GMT</pubDate>
    <dc:creator>hajsenberg22</dc:creator>
    <dc:date>2025-08-24T19:37:53Z</dc:date>
    <item>
      <title>Dimmer with MC68HC908QT4CP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2157087#M24208</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Following this article&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2839.pdf" target="_blank"&gt;AN2839: Implementing a Lamp Dimmer with an HC908Q Family MCU&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I got&amp;nbsp;MC68HC908QT4CP.&lt;BR /&gt;&lt;BR /&gt;I am looking for programmator and application to support it, I got the code from the nxp article above.&lt;BR /&gt;&lt;BR /&gt;Looking at this forum, I could use CodeWarrior Dev Studio v11 or CodeWarrior Classic 6.3?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;What else I would need to get that code into chip:&amp;nbsp;USBMULTILINK08,&amp;nbsp;M68CPA08P40B56, anything else? I have ALL-07 but don't think it supports it.&lt;BR /&gt;&lt;BR /&gt;Thanks&amp;nbsp;&lt;BR /&gt;hajsenberg&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 24 Aug 2025 19:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2157087#M24208</guid>
      <dc:creator>hajsenberg22</dc:creator>
      <dc:date>2025-08-24T19:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: Dimmer with MC68HC908QT4CP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2157728#M24209</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254064"&gt;@hajsenberg22&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;For HC08QT4, we recommend using CodeWarrior 6.3 as IDE.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/codewarrior-development-tools/codewarrior-legacy/codewarrior-for-microcontrollers-classic-ide-rs08-hcs08-coldfire-v1-v6-3:CW-MICROCONTROLLERS" target="_blank"&gt;CodeWarrior® for Microcontrollers-Classic IDE | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For programmer you can take a look to PEmicro Cyclone FX programmer which still support HC08 devices.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/CYCLONE-FX" target="_blank"&gt;PEmicro Cyclone FX programmer | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 18:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2157728#M24209</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-08-25T18:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: Dimmer with MC68HC908QT4CP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2161557#M24214</link>
      <description>&lt;P&gt;HI Pablo, thank you for the message.&lt;/P&gt;&lt;P&gt;Today is relatively hard to find HC908 &amp;amp; programmer, and I was wondering is there any other microchip from NXP which could work in a same way &amp;amp; with same code from that datasheet -&amp;gt; with some other more popular programmer &amp;amp; new versions of CodeWarrior?&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Leon&lt;/P&gt;</description>
      <pubDate>Mon, 01 Sep 2025 18:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2161557#M24214</guid>
      <dc:creator>hajsenberg22</dc:creator>
      <dc:date>2025-09-01T18:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: Dimmer with MC68HC908QT4CP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2164594#M24218</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254064"&gt;@hajsenberg22&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I apologize for the inconvenience this may cause you, but the MC68HC908QT4CP does not have a direct replacement.&lt;/P&gt;
&lt;P&gt;If you want to stay within the 8-bit family, I recommend exploring the S08 MCU portfolio, however, they are not software compatible with the MC68HC908QT4CP. Specifically, the S08PB series is a good starting point, as it offers evaluation and development boards.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit-s08-mcus:HCS08" target="_blank"&gt;8-Bit S08 MCUs | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/S08PB16-EVK" target="_blank"&gt;S08PB16 and S08PLS Evaluation Kit | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The S08 MCUs use CodeWarrior 11.1 as the development IDE. You can program them using various tools such as:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/universal-multilink-development-interface:UMultilink" target="_blank"&gt;Universal Multilink Development Interface | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/CYCLONE-FX" target="_blank"&gt;PEmicro Cyclone FX programmer | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/U-MULTILINK-FX" target="_blank"&gt;Universal Multilink FX High-Speed Development Interface | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/CYCLONE" target="_blank"&gt;PEmicro Cyclone programmer | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you use the Evaluation Kit, it comes with OSBDM, which allows you to flash and debug the MCU without needing an external debug tool.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Fri, 05 Sep 2025 21:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Dimmer-with-MC68HC908QT4CP/m-p/2164594#M24218</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-09-05T21:17:44Z</dc:date>
    </item>
  </channel>
</rss>