<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08SH obsolete info in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH-obsolete-info/m-p/2133554#M24188</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250165"&gt;@anandhram1988&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The differences between the S08SH, S08SG, and S08EL are as follows:&lt;/P&gt;
&lt;P&gt;S08EL includes the SLIC peripheral, which supports LIN 2.0 and SAE J2602 protocols. It also features 16 interrupt pins and up to 512 bytes of EEPROM.&lt;/P&gt;
&lt;P&gt;S08SH features the MTIM peripheral, has only 8 interrupt pins, and supports a ganged output option that allows a single write to change the state of multiple pins simultaneously.&lt;/P&gt;
&lt;P&gt;S08SG is similar to the S08SH in terms of pinout, tools, and software compatibility. However, it offers a wider range of package options.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
    <pubDate>Mon, 14 Jul 2025 21:49:40 GMT</pubDate>
    <dc:creator>Pablo_Ramos</dc:creator>
    <dc:date>2025-07-14T21:49:40Z</dc:date>
    <item>
      <title>MC9S08SH obsolete info</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH-obsolete-info/m-p/2131791#M24186</link>
      <description>&lt;P&gt;hi, anybody can inform please the direct replacement for&amp;nbsp;MC9S08SH32 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i found below,&amp;nbsp;MC9S08SG32 and&amp;nbsp;MC9S08EL32&lt;/P&gt;&lt;P&gt;in this case i would like to know the main differences between&amp;nbsp;&lt;/P&gt;&lt;P&gt;MC9S08SH32 vs&amp;nbsp;&amp;nbsp;MC9S08SG32&amp;nbsp; vs&amp;nbsp;MC9S08EL32&lt;/P&gt;&lt;P&gt;Many thanks in advance&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 15:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH-obsolete-info/m-p/2131791#M24186</guid>
      <dc:creator>anandhram1988</dc:creator>
      <dc:date>2025-07-10T15:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH obsolete info</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH-obsolete-info/m-p/2133554#M24188</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250165"&gt;@anandhram1988&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The differences between the S08SH, S08SG, and S08EL are as follows:&lt;/P&gt;
&lt;P&gt;S08EL includes the SLIC peripheral, which supports LIN 2.0 and SAE J2602 protocols. It also features 16 interrupt pins and up to 512 bytes of EEPROM.&lt;/P&gt;
&lt;P&gt;S08SH features the MTIM peripheral, has only 8 interrupt pins, and supports a ganged output option that allows a single write to change the state of multiple pins simultaneously.&lt;/P&gt;
&lt;P&gt;S08SG is similar to the S08SH in terms of pinout, tools, and software compatibility. However, it offers a wider range of package options.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jul 2025 21:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH-obsolete-info/m-p/2133554#M24188</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-07-14T21:49:40Z</dc:date>
    </item>
  </channel>
</rss>