<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC705C8ACPE vs MC68HC705ACP? Is the only difference RoHS? Drop in replacement?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC705C8ACPE-vs-MC68HC705ACP-Is-the-only-difference-RoHS-Drop-in/m-p/2128421#M24184</link>
    <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;Can anyone tell me if these 2 parts are truly compatible? I've seen where someone has said the number minus the infamous 68HC but with the E suffix is just the RoHS version. If that's the case why not just add the E to an already existing number that has been around for literally decades? When looking up the MC705C8 on a franchise site, the link to the datasheet always brings up the 68HC datasheet. So I'm a bit lost on what&amp;nbsp;&lt;A href="https://www.dogwhistles.net" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;dog whistles app&lt;/FONT&gt;&lt;/A&gt; is true and what is not. Any help appreciated. Thank you&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the MC705C8 and MC68HC705C8E are highly compatible. The "68HC" prefix is often implied or dropped for the 705 series, which predominantly uses High-Speed CMOS technology. The "E" suffix typically denotes a RoHS-compliant version, meaning it meets environmental standards but is functionally identical to the non-E version. Manufacturers usually maintain a single datasheet (like for the MC68HC705C8) for these core parts, covering all minor variations. In essence, you can consider them interchangeable for most applications.&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jul 2025 05:44:31 GMT</pubDate>
    <dc:creator>marilyn55david</dc:creator>
    <dc:date>2025-07-04T05:44:31Z</dc:date>
    <item>
      <title>MC705C8ACPE vs MC68HC705ACP? Is the only difference RoHS? Drop in replacement?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC705C8ACPE-vs-MC68HC705ACP-Is-the-only-difference-RoHS-Drop-in/m-p/2072948#M24145</link>
      <description>&lt;P&gt;Can anyone tell me if these 2 parts are truly compatible? I've seen where someone has said the number minus the infamous 68HC but with the E suffix is just the RoHS version. If that's the case why not just add the E to an already existing number that has been around for literally decades? When looking up the MC705C8 on a franchise site, the link to the datasheet always brings up the 68HC datasheet. So I'm a bit lost on what is true and what is not. Any help appreciated. Thank you&lt;/P&gt;</description>
      <pubDate>Wed, 02 Apr 2025 14:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC705C8ACPE-vs-MC68HC705ACP-Is-the-only-difference-RoHS-Drop-in/m-p/2072948#M24145</guid>
      <dc:creator>CROSSCOMPONENTSQC</dc:creator>
      <dc:date>2025-04-02T14:44:33Z</dc:date>
    </item>
    <item>
      <title>Re: MC705C8ACPE vs MC68HC705ACP? Is the only difference RoHS? Drop in replacement?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC705C8ACPE-vs-MC68HC705ACP-Is-the-only-difference-RoHS-Drop-in/m-p/2128421#M24184</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;Can anyone tell me if these 2 parts are truly compatible? I've seen where someone has said the number minus the infamous 68HC but with the E suffix is just the RoHS version. If that's the case why not just add the E to an already existing number that has been around for literally decades? When looking up the MC705C8 on a franchise site, the link to the datasheet always brings up the 68HC datasheet. So I'm a bit lost on what&amp;nbsp;&lt;A href="https://www.dogwhistles.net" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;dog whistles app&lt;/FONT&gt;&lt;/A&gt; is true and what is not. Any help appreciated. Thank you&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the MC705C8 and MC68HC705C8E are highly compatible. The "68HC" prefix is often implied or dropped for the 705 series, which predominantly uses High-Speed CMOS technology. The "E" suffix typically denotes a RoHS-compliant version, meaning it meets environmental standards but is functionally identical to the non-E version. Manufacturers usually maintain a single datasheet (like for the MC68HC705C8) for these core parts, covering all minor variations. In essence, you can consider them interchangeable for most applications.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jul 2025 05:44:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC705C8ACPE-vs-MC68HC705ACP-Is-the-only-difference-RoHS-Drop-in/m-p/2128421#M24184</guid>
      <dc:creator>marilyn55david</dc:creator>
      <dc:date>2025-07-04T05:44:31Z</dc:date>
    </item>
  </channel>
</rss>