<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Deciphering markings on a mask-programmed HC11 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2092476#M24160</link>
    <description>&lt;P&gt;I've had this board kicking around for a while that has a Motorola processor on it (in a PLCC-52 form factor).&lt;/P&gt;
&lt;P&gt;I recently realized that it is actually a mask-programmed version of the 68HC11E9.&lt;/P&gt;
&lt;P&gt;There are some additional markings on the chip, and I just want to verify that they would include the firmware that would have been masked into the chip at the time of manufacture.&lt;/P&gt;
&lt;P&gt;Note: Some information on this thread has been removed as it may contain sensitive information.&lt;/P&gt;</description>
    <pubDate>Mon, 12 May 2025 16:46:04 GMT</pubDate>
    <dc:creator>meterman1980</dc:creator>
    <dc:date>2025-05-12T16:46:04Z</dc:date>
    <item>
      <title>Deciphering markings on a mask-programmed HC11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2092476#M24160</link>
      <description>&lt;P&gt;I've had this board kicking around for a while that has a Motorola processor on it (in a PLCC-52 form factor).&lt;/P&gt;
&lt;P&gt;I recently realized that it is actually a mask-programmed version of the 68HC11E9.&lt;/P&gt;
&lt;P&gt;There are some additional markings on the chip, and I just want to verify that they would include the firmware that would have been masked into the chip at the time of manufacture.&lt;/P&gt;
&lt;P&gt;Note: Some information on this thread has been removed as it may contain sensitive information.&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 16:46:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2092476#M24160</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2025-05-12T16:46:04Z</dc:date>
    </item>
    <item>
      <title>Re: Deciphering markings on a mask-programmed HC11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2092975#M24161</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/130597"&gt;@meterman1980&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;For marking information, please contact your Authorized NXP Representative.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Wed, 07 May 2025 17:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2092975#M24161</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2025-05-07T17:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: Deciphering markings on a mask-programmed HC11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2095507#M24162</link>
      <description>&lt;P&gt;I don't even have an authorized rep. I'm just a hobbyist.&lt;/P&gt;&lt;P&gt;I eventually got my answer elsewhere.&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 12:28:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Deciphering-markings-on-a-mask-programmed-HC11/m-p/2095507#M24162</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2025-05-12T12:28:53Z</dc:date>
    </item>
  </channel>
</rss>