<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Can't init device hci0: Connection timed out (110)</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-init-device-hci0-Connection-timed-out-110/m-p/2038325#M24115</link>
    <description>&lt;P&gt;Is there any error message during the boot up? Is the driver loading correct?&lt;/P&gt;
&lt;P&gt;e.g. is the path of the firmware incorrect? are the gpio pins for controlling the chip is properly?&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What is the setup in your board device tree?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 05 Feb 2025 07:15:21 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2025-02-05T07:15:21Z</dc:date>
    <item>
      <title>Can't init device hci0: Connection timed out (110)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-init-device-hci0-Connection-timed-out-110/m-p/2037584#M24114</link>
      <description>&lt;P&gt;I'm am working with imx93 board in Linux 6.6.52&lt;BR /&gt;&lt;BR /&gt;I have used below&amp;nbsp; commands to enable BT interfcae&lt;/P&gt;&lt;P&gt;modprobe moal mod_para=nxp/wifi_mod_para.conf&lt;BR /&gt;modprobe btnxpuart&lt;/P&gt;&lt;P&gt;hciconfig hci0 up&lt;BR /&gt;Can't init device hci0: Connection timed out (110)&lt;BR /&gt;and Im getting error like this&lt;BR /&gt;BT module name -LBEE5PL2DL-921&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 08:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-init-device-hci0-Connection-timed-out-110/m-p/2037584#M24114</guid>
      <dc:creator>Ashwini_A</dc:creator>
      <dc:date>2025-02-04T08:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: Can't init device hci0: Connection timed out (110)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-init-device-hci0-Connection-timed-out-110/m-p/2038325#M24115</link>
      <description>&lt;P&gt;Is there any error message during the boot up? Is the driver loading correct?&lt;/P&gt;
&lt;P&gt;e.g. is the path of the firmware incorrect? are the gpio pins for controlling the chip is properly?&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What is the setup in your board device tree?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 07:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-init-device-hci0-Connection-timed-out-110/m-p/2038325#M24115</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-02-05T07:15:21Z</dc:date>
    </item>
  </channel>
</rss>