<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 there is no input and output interaction</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/there-is-no-input-and-output-interaction/m-p/2020064#M24094</link>
    <description>&lt;P&gt;Why can the microcontroller program be debuged normally, but there is no input and output interaction？All processes are fine, but there is no response after the program is written in. And there are no values in the debugger.&lt;/P&gt;</description>
    <pubDate>Fri, 27 Dec 2024 12:23:46 GMT</pubDate>
    <dc:creator>Li9999</dc:creator>
    <dc:date>2024-12-27T12:23:46Z</dc:date>
    <item>
      <title>there is no input and output interaction</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/there-is-no-input-and-output-interaction/m-p/2020064#M24094</link>
      <description>&lt;P&gt;Why can the microcontroller program be debuged normally, but there is no input and output interaction？All processes are fine, but there is no response after the program is written in. And there are no values in the debugger.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Dec 2024 12:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/there-is-no-input-and-output-interaction/m-p/2020064#M24094</guid>
      <dc:creator>Li9999</dc:creator>
      <dc:date>2024-12-27T12:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: there is no input and output interaction</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/there-is-no-input-and-output-interaction/m-p/2020590#M24096</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238073"&gt;@Li9999&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you help me with the following information?&lt;/P&gt;
&lt;P&gt;Which MCU and debugger are you using?&lt;/P&gt;
&lt;P&gt;What version of CodeWarrior are you using?&lt;/P&gt;
&lt;P&gt;Also, could you explain furthermore what is the expected behavior of the application?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Dec 2024 23:45:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/there-is-no-input-and-output-interaction/m-p/2020590#M24096</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2024-12-30T23:45:03Z</dc:date>
    </item>
  </channel>
</rss>