<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unknown Base plugin Nub error in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1972727#M24057</link>
    <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I have a project in Code Warrior 10.6.4 IDE developed for&amp;nbsp;MC9S08QE128 MCU.&lt;/P&gt;&lt;P&gt;I am using PE micro Multilink FX as a debugger and programmer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;until a week ago I was able to debug and burn the code. to the flash of the MCU with no problem.&lt;/P&gt;&lt;P&gt;now when i try to debug or burn the code i get the error "Unknown Base Plugin Nub error".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;with the PROGHCS08 - Flash Programmer Software from PE micro i have no problem burning the code on the board with the same debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;when checking the signal of the BDM, i can see that the PC tried to initiate connection with the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;have anyone faced this problem and can help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;omer&lt;/P&gt;</description>
    <pubDate>Sun, 13 Oct 2024 11:21:51 GMT</pubDate>
    <dc:creator>tcherno</dc:creator>
    <dc:date>2024-10-13T11:21:51Z</dc:date>
    <item>
      <title>Unknown Base plugin Nub error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1972727#M24057</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I have a project in Code Warrior 10.6.4 IDE developed for&amp;nbsp;MC9S08QE128 MCU.&lt;/P&gt;&lt;P&gt;I am using PE micro Multilink FX as a debugger and programmer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;until a week ago I was able to debug and burn the code. to the flash of the MCU with no problem.&lt;/P&gt;&lt;P&gt;now when i try to debug or burn the code i get the error "Unknown Base Plugin Nub error".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;with the PROGHCS08 - Flash Programmer Software from PE micro i have no problem burning the code on the board with the same debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;when checking the signal of the BDM, i can see that the PC tried to initiate connection with the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;have anyone faced this problem and can help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;omer&lt;/P&gt;</description>
      <pubDate>Sun, 13 Oct 2024 11:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1972727#M24057</guid>
      <dc:creator>tcherno</dc:creator>
      <dc:date>2024-10-13T11:21:51Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown Base plugin Nub error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1974615#M24059</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241886"&gt;@tcherno&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I noticed that you already made a similar question on other community post. There is some activity in said post so please follow up there. I’m adding a link here for reference of other community users that may find it helpful.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-Development-Tools/Unknown-Base-Plugin-Nub-error/td-p/1972726" target="_blank"&gt;Unknown Base Plugin Nub error - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 21:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1974615#M24059</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2024-10-15T21:48:13Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown Base plugin Nub error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1982695#M24067</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Restart CodeWarrior and reconnect the Multilink FX. Update P&amp;amp;E drivers for CodeWarrior and Multilink FX. Reset debug settings (Project &amp;gt; Properties &amp;gt; Debug/Launch Settings) and clear the workspace cache by deleting the .metadata folder.&lt;/P&gt;&lt;P&gt;thanks and regards&lt;BR /&gt;pawantanwar&lt;BR /&gt;&lt;A href="https://www.multispanindia.com" target="_blank"&gt;https://www.multispanindia.com&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 06:01:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unknown-Base-plugin-Nub-error/m-p/1982695#M24067</guid>
      <dc:creator>pawantanwar</dc:creator>
      <dc:date>2024-10-28T06:01:47Z</dc:date>
    </item>
  </channel>
</rss>