<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IEC 60730 Class B Safety Library for S08PT60 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IEC-60730-Class-B-Safety-Library-for-S08PT60/m-p/1886745#M23906</link>
    <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;1) Is there an&amp;nbsp;IEC 60730 Class B Safety Library for S08PT60 ?&lt;/P&gt;&lt;P&gt;2) Is it easy to port the&amp;nbsp;IEC 60730 Class B Safety Library from S08PBxx to S08PT60 ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carl&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jun 2024 07:57:20 GMT</pubDate>
    <dc:creator>CarlLee</dc:creator>
    <dc:date>2024-06-13T07:57:20Z</dc:date>
    <item>
      <title>IEC 60730 Class B Safety Library for S08PT60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IEC-60730-Class-B-Safety-Library-for-S08PT60/m-p/1886745#M23906</link>
      <description>&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;1) Is there an&amp;nbsp;IEC 60730 Class B Safety Library for S08PT60 ?&lt;/P&gt;&lt;P&gt;2) Is it easy to port the&amp;nbsp;IEC 60730 Class B Safety Library from S08PBxx to S08PT60 ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carl&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 07:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IEC-60730-Class-B-Safety-Library-for-S08PT60/m-p/1886745#M23906</guid>
      <dc:creator>CarlLee</dc:creator>
      <dc:date>2024-06-13T07:57:20Z</dc:date>
    </item>
    <item>
      <title>Re: IEC 60730 Class B Safety Library for S08PT60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IEC-60730-Class-B-Safety-Library-for-S08PT60/m-p/1889796#M23910</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205968"&gt;@CarlLee&lt;/a&gt;,&lt;BR /&gt;No, there is no IEC 60730 Class B Safety library for S08PT60, also there is no documentation regarding a port from S08PBxx to S08PT60. &lt;BR /&gt;A recommendation could be to check the difference between both processor in order to see if a change in the IEC 60730 Class B Safety library is necessary.&lt;/P&gt;
&lt;P&gt;An apology for the inconvenience.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 21:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IEC-60730-Class-B-Safety-Library-for-S08PT60/m-p/1889796#M23910</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2024-06-18T21:10:14Z</dc:date>
    </item>
  </channel>
</rss>