<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: secure byte of MC908QY4ACDWE ..</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/secure-byte-of-MC908QY4ACDWE/m-p/1849233#M23885</link>
    <description>I see that this request is related to a support ticket that was submited by your Sales contact Kelvin Lee at AVNET, right?&lt;BR /&gt;We'll continue the troubleshooting through that support case to speed up the process. Therefore, please keep in touch with him.&lt;BR /&gt;&lt;BR /&gt;Thanks for your patience!&lt;BR /&gt;&lt;BR /&gt;NOTE: Once we complete the troubleshooting and find the root cause of the error I'll also post the final solution in this post as well</description>
    <pubDate>Wed, 17 Apr 2024 17:54:32 GMT</pubDate>
    <dc:creator>Itzzamna_Supp</dc:creator>
    <dc:date>2024-04-17T17:54:32Z</dc:date>
    <item>
      <title>secure byte of MC908QY4ACDWE ..</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/secure-byte-of-MC908QY4ACDWE/m-p/1840142#M23872</link>
      <description>&lt;P&gt;Hello Technical Support Team,&lt;/P&gt;&lt;P&gt;I have five ICs (Freescale MC908QY4ACDWE), which are unable to access flash memory. When I use a key of 8 bytes with all FF, and read RAM address 80h, I get a value of 0x3F, which seems to be incorrect.&lt;/P&gt;&lt;P&gt;Could you please provide the default factory key value? Are there any other available key values?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 09:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/secure-byte-of-MC908QY4ACDWE/m-p/1840142#M23872</guid>
      <dc:creator>trevorlin</dc:creator>
      <dc:date>2024-04-03T09:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: secure byte of MC908QY4ACDWE ..</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/secure-byte-of-MC908QY4ACDWE/m-p/1849233#M23885</link>
      <description>I see that this request is related to a support ticket that was submited by your Sales contact Kelvin Lee at AVNET, right?&lt;BR /&gt;We'll continue the troubleshooting through that support case to speed up the process. Therefore, please keep in touch with him.&lt;BR /&gt;&lt;BR /&gt;Thanks for your patience!&lt;BR /&gt;&lt;BR /&gt;NOTE: Once we complete the troubleshooting and find the root cause of the error I'll also post the final solution in this post as well</description>
      <pubDate>Wed, 17 Apr 2024 17:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/secure-byte-of-MC908QY4ACDWE/m-p/1849233#M23885</guid>
      <dc:creator>Itzzamna_Supp</dc:creator>
      <dc:date>2024-04-17T17:54:32Z</dc:date>
    </item>
  </channel>
</rss>