<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: File .CRT</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/File-CRT/m-p/1805417#M23843</link>
    <description>When compiling, S19 is generated and remains in the FLASH folder, the SRecord file type is saved there in S19, where you will find the CRT.</description>
    <pubDate>Mon, 12 Feb 2024 17:50:08 GMT</pubDate>
    <dc:creator>Itzzamna_Supp</dc:creator>
    <dc:date>2024-02-12T17:50:08Z</dc:date>
    <item>
      <title>File .CRT</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/File-CRT/m-p/1804481#M23842</link>
      <description>&lt;P&gt;I'm trying to create a .CRT file in Code Warrior Classic from a .S19 file.&lt;/P&gt;&lt;P&gt;Is it possible or this standard .CRT is not public and I need some specific SW and some parameters?&lt;/P&gt;&lt;P&gt;Is it possible with Code Warrior Ecilpse?&lt;/P&gt;&lt;P&gt;What are the basic differences in .S19 and .CRT standars to flash a MC9S08AW32 ?&lt;/P&gt;&lt;P&gt;Can I use both for the same purpose ?&lt;/P&gt;</description>
      <pubDate>Fri, 09 Feb 2024 01:24:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/File-CRT/m-p/1804481#M23842</guid>
      <dc:creator>FabioPdM</dc:creator>
      <dc:date>2024-02-09T01:24:04Z</dc:date>
    </item>
    <item>
      <title>Re: File .CRT</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/File-CRT/m-p/1805417#M23843</link>
      <description>When compiling, S19 is generated and remains in the FLASH folder, the SRecord file type is saved there in S19, where you will find the CRT.</description>
      <pubDate>Mon, 12 Feb 2024 17:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/File-CRT/m-p/1805417#M23843</guid>
      <dc:creator>Itzzamna_Supp</dc:creator>
      <dc:date>2024-02-12T17:50:08Z</dc:date>
    </item>
  </channel>
</rss>