<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is CW v11.1 working with Windows 11 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1787279#M23826</link>
    <description>&lt;P&gt;This should be tested for WIN11, is Driver for the CW TAP updated?&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jan 2024 14:29:35 GMT</pubDate>
    <dc:creator>jodavmo</dc:creator>
    <dc:date>2024-01-11T14:29:35Z</dc:date>
    <item>
      <title>Is CW v11.1 working with Windows 11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1382627#M23440</link>
      <description>&lt;P&gt;Dear Community&lt;/P&gt;&lt;P&gt;I am working with Code Warrior v11.1 and DEMO9S08QG8 board on a computer with Windows 10.&lt;BR /&gt;But now Windows 10 is being replaced by Windows 11 and I have to ask myself, can I work with CW v11.1 and the new Windows 11 again.&lt;/P&gt;&lt;P&gt;Can somebody please say me something about it?&lt;/P&gt;&lt;P&gt;With best regards&lt;/P&gt;&lt;P&gt;Gerd&lt;/P&gt;</description>
      <pubDate>Tue, 07 Dec 2021 11:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1382627#M23440</guid>
      <dc:creator>Mei</dc:creator>
      <dc:date>2021-12-07T11:28:15Z</dc:date>
    </item>
    <item>
      <title>Re: Is CW v11.1 working with Windows 11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1383615#M23444</link>
      <description>&lt;P&gt;Sorry I do not have window 11 yet, but as far I know codewarrior 11.1 has not been tested on windows 11&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Vicente&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 22:53:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1383615#M23444</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-12-08T22:53:32Z</dc:date>
    </item>
    <item>
      <title>Re: Is CW v11.1 working with Windows 11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1384209#M23447</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;Thank you for your reponse. &lt;BR /&gt;But I'm not worried, because yesterday I heard in my internet club that Windows 10 &lt;BR /&gt;will be updated for a long time. &lt;/SPAN&gt;&lt;SPAN class=""&gt;So I can continue to work with it.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;With best regards&lt;BR /&gt;Gerd&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Dec 2021 18:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1384209#M23447</guid>
      <dc:creator>Mei</dc:creator>
      <dc:date>2021-12-09T18:18:34Z</dc:date>
    </item>
    <item>
      <title>Re: Is CW v11.1 working with Windows 11</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1787279#M23826</link>
      <description>&lt;P&gt;This should be tested for WIN11, is Driver for the CW TAP updated?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 14:29:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Is-CW-v11-1-working-with-Windows-11/m-p/1787279#M23826</guid>
      <dc:creator>jodavmo</dc:creator>
      <dc:date>2024-01-11T14:29:35Z</dc:date>
    </item>
  </channel>
</rss>