<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flash programming MC9S08QG8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flash-programming-MC9S08QG8/m-p/1763582#M23808</link>
    <description>&lt;PRE&gt;&lt;SPAN class=""&gt;Dear Community&lt;BR /&gt;I wrote an assembler program to store data in the flash of MC9S08QG8. &lt;BR /&gt;It still has errors. The program allows one byte to be saved &lt;BR /&gt;in a program loop in BDM debug mode, &lt;BR /&gt;but not several bytes continuously. &lt;BR /&gt;The required NOPs at the end of the programming loop are also not OK. &lt;BR /&gt;Can you help me?&lt;/SPAN&gt;&lt;/PRE&gt;</description>
    <pubDate>Sat, 25 Nov 2023 19:06:35 GMT</pubDate>
    <dc:creator>Mei</dc:creator>
    <dc:date>2023-11-25T19:06:35Z</dc:date>
    <item>
      <title>Flash programming MC9S08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flash-programming-MC9S08QG8/m-p/1763582#M23808</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;Dear Community&lt;BR /&gt;I wrote an assembler program to store data in the flash of MC9S08QG8. &lt;BR /&gt;It still has errors. The program allows one byte to be saved &lt;BR /&gt;in a program loop in BDM debug mode, &lt;BR /&gt;but not several bytes continuously. &lt;BR /&gt;The required NOPs at the end of the programming loop are also not OK. &lt;BR /&gt;Can you help me?&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Sat, 25 Nov 2023 19:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flash-programming-MC9S08QG8/m-p/1763582#M23808</guid>
      <dc:creator>Mei</dc:creator>
      <dc:date>2023-11-25T19:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming MC9S08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flash-programming-MC9S08QG8/m-p/1816813#M23847</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;Now I have implemented my Flash program for writing bytes and &lt;BR /&gt;deleting byte blocks in assembly code.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;The community helped me with this, but I don't know how to &lt;BR /&gt;give kudos to the answer authors.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Another interesting observation when using the Flash routine:
When I test the routine with a chip that has been used for a long time,&lt;BR /&gt;it happens that some bytes in the deleted block are not deleted.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;If I write and delete in a higher, less used program area, &lt;BR /&gt;this doesn't happen.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;STRONG&gt;Thank you to the community&lt;BR /&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Next time I would like to ask my questions about transferring &lt;BR /&gt;the measured values ​​to a PC.&lt;BR /&gt;With best regards&lt;BR /&gt;Gerd&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Tue, 27 Feb 2024 20:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flash-programming-MC9S08QG8/m-p/1816813#M23847</guid>
      <dc:creator>Mei</dc:creator>
      <dc:date>2024-02-27T20:15:54Z</dc:date>
    </item>
  </channel>
</rss>