<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1693217#M23763</link>
    <description>&lt;P&gt;yes both has normally the same mask set&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 26 Jul 2023 16:09:22 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2023-07-26T16:09:22Z</dc:date>
    <item>
      <title>MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1689605#M23755</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i need to rebuild some command electronic cards (builded in 2014) with two MCU type&amp;nbsp;&lt;SPAN class=""&gt;&lt;SPAN&gt;MC9S08DZ60 AMLH (8bit)&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;These MCU's are not easy to found and buy now and will require many mounth to be delivered from NXP.&lt;/P&gt;&lt;P&gt;The MCU S9S08DZ60 F2MLH (8 bit) are equivalent or is it better not to use them for the project??&lt;/P&gt;&lt;P&gt;The functions used are simple, and the Can Bus port is used to connect to other units (to send inputs status and to receive led outputs status).&lt;BR /&gt;Has anyone had a chance to use them and can provide advice?&lt;/P&gt;&lt;P&gt;Thanks for the information,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 16:46:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1689605#M23755</guid>
      <dc:creator>spa66</dc:creator>
      <dc:date>2023-07-20T16:46:34Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1689779#M23756</link>
      <description>&lt;P&gt;the MC9S08DZ is the commercial version of the S9S08DZ&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Both parts have the same features you only need to check the errata for the two differents mask set, you can check the errata on the next link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit-s08-mcus/8-bit-cost-effective-with-can-d-mcus:S08D" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit-s08-mcus/8-bit-cost-effective-with-can-d-mcus:S08D&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;vicente&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jul 2023 22:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1689779#M23756</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-07-20T22:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1690092#M23757</link>
      <description>&lt;P&gt;Hi Vincent,&lt;/P&gt;&lt;P&gt;thank you for reply.&lt;/P&gt;&lt;P&gt;Could you clarify me what mask is corrispondent to the letters in the CPU's code?&lt;/P&gt;&lt;P&gt;A = ...;&lt;/P&gt;&lt;P&gt;F1= ....;&lt;/P&gt;&lt;P&gt;F2=....;&lt;/P&gt;&lt;P&gt;Thank you for the answers.&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jul 2023 06:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1690092#M23757</guid>
      <dc:creator>spa66</dc:creator>
      <dc:date>2023-07-21T06:42:22Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1690541#M23758</link>
      <description>&lt;TABLE width="179"&gt;
&lt;TBODY&gt;
&lt;TR&gt;
&lt;TD width="115"&gt;S9S08DZ60F2MLH&lt;/TD&gt;
&lt;TD width="64"&gt;2M74K&amp;nbsp;&lt;/TD&gt;
&lt;/TR&gt;
&lt;TR&gt;
&lt;TD&gt;S9S08DZ60F1MLH&lt;/TD&gt;
&lt;TD&gt;no longer manufacturer&lt;/TD&gt;
&lt;/TR&gt;
&lt;/TBODY&gt;
&lt;/TABLE&gt;
&lt;P&gt;the F2 is mask set 2M74K&lt;/P&gt;
&lt;P&gt;the F1 is no longer manufacturer&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jul 2023 16:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1690541#M23758</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-07-21T16:11:26Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1690728#M23759</link>
      <description>&lt;P&gt;Hi Vincente,&lt;/P&gt;&lt;P&gt;Ok, for the new:&lt;/P&gt;&lt;TABLE width="179"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD width="115"&gt;S9S08DZ60F2MLH&lt;/TD&gt;&lt;TD width="64"&gt;2M74K&amp;nbsp;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but the type:&lt;/P&gt;&lt;P&gt;MC9S08DZ60 AMLH&lt;/P&gt;&lt;P&gt;which mask have?&lt;/P&gt;&lt;P&gt;Thank you for reply.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 22 Jul 2023 14:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1690728#M23759</guid>
      <dc:creator>spa66</dc:creator>
      <dc:date>2023-07-22T14:13:20Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1692447#M23760</link>
      <description>&lt;P&gt;normally the&amp;nbsp; MC9S08DZ60AMLH is&amp;nbsp;&lt;SPAN&gt;2M74K, but you can check it on the body mark of the device on the second line&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 18:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1692447#M23760</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-07-25T18:54:22Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1692449#M23761</link>
      <description>&lt;P&gt;Hi Vincente,&lt;/P&gt;&lt;P&gt;but that means MC9S08DZ60 AMLH and S9S08DZ60 F2MLH,&lt;/P&gt;&lt;P&gt;with the same mask 2M74K are equivalents.&lt;/P&gt;&lt;P&gt;So we can buy the S9S08DZ60 F2MLH to replace the&amp;nbsp;MC9S08DZ60 AMLH!&lt;/P&gt;&lt;P&gt;This is true or I have not understood?&lt;/P&gt;&lt;P&gt;Thank you for reply,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 19:02:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1692449#M23761</guid>
      <dc:creator>spa66</dc:creator>
      <dc:date>2023-07-25T19:02:41Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DZ60 AMLH Vs S9S08DZ60 F2MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1693217#M23763</link>
      <description>&lt;P&gt;yes both has normally the same mask set&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jul 2023 16:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DZ60-AMLH-Vs-S9S08DZ60-F2MLH/m-p/1693217#M23763</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-07-26T16:09:22Z</dc:date>
    </item>
  </channel>
</rss>