<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Help with using TSN from 1028ardb via putty</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-with-using-TSN-from-1028ardb-via-putty/m-p/1638853#M23704</link>
    <description>&lt;P&gt;To use the TSN (Time-Sensitive Networking) and QBV (Quality of Service Basic Mode) features on the 1028ardb board via PuTTY, you first need to establish a serial connection between your computer and the board. Here are the steps to do so:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Connect the serial cable to your computer's serial port or USB-to-serial adapter.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Open PuTTY and go to the "Serial" category under the "Connection" tab.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Under the "Serial line" field, enter the serial port number that corresponds to your serial connection (e.g. COM1 or /dev/ttyS0).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Set the baud rate to 115200 (or whatever baud rate is specified by the 1028ardb board manual).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Click on the "Open" button to open the serial connection.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Once you have established the serial connection, you can access the TSN and QBV features by using the command-line interface of the 1028ardb board. You may refer to the board's manual for the specific commands needed to enable and configure these features.&lt;/P&gt;&lt;P&gt;Hope &lt;A title="supplier" href="https://www.perceptive-ic.com/" target="_blank" rel="noopener"&gt;help&lt;/A&gt;.&lt;/P&gt;</description>
    <pubDate>Mon, 24 Apr 2023 10:19:00 GMT</pubDate>
    <dc:creator>CarrieDuoduo</dc:creator>
    <dc:date>2023-04-24T10:19:00Z</dc:date>
    <item>
      <title>Help with using TSN from 1028ardb via putty</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-with-using-TSN-from-1028ardb-via-putty/m-p/1627653#M23697</link>
      <description>&lt;P&gt;I want to use qbv feature on putty.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 11:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-with-using-TSN-from-1028ardb-via-putty/m-p/1627653#M23697</guid>
      <dc:creator>nhanthanh</dc:creator>
      <dc:date>2023-04-04T11:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: Help with using TSN from 1028ardb via putty</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-with-using-TSN-from-1028ardb-via-putty/m-p/1638853#M23704</link>
      <description>&lt;P&gt;To use the TSN (Time-Sensitive Networking) and QBV (Quality of Service Basic Mode) features on the 1028ardb board via PuTTY, you first need to establish a serial connection between your computer and the board. Here are the steps to do so:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Connect the serial cable to your computer's serial port or USB-to-serial adapter.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Open PuTTY and go to the "Serial" category under the "Connection" tab.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Under the "Serial line" field, enter the serial port number that corresponds to your serial connection (e.g. COM1 or /dev/ttyS0).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Set the baud rate to 115200 (or whatever baud rate is specified by the 1028ardb board manual).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Click on the "Open" button to open the serial connection.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Once you have established the serial connection, you can access the TSN and QBV features by using the command-line interface of the 1028ardb board. You may refer to the board's manual for the specific commands needed to enable and configure these features.&lt;/P&gt;&lt;P&gt;Hope &lt;A title="supplier" href="https://www.perceptive-ic.com/" target="_blank" rel="noopener"&gt;help&lt;/A&gt;.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Apr 2023 10:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-with-using-TSN-from-1028ardb-via-putty/m-p/1638853#M23704</guid>
      <dc:creator>CarrieDuoduo</dc:creator>
      <dc:date>2023-04-24T10:19:00Z</dc:date>
    </item>
  </channel>
</rss>