<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Acceptance Mask MC9S08DZ96MLH in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Acceptance-Mask-MC9S08DZ96MLH/m-p/1629694#M23698</link>
    <description>&lt;P&gt;Hi, I am using the MC9S08DZ96MLH chip in a project. In this project, this chip receives messages with the following identifiers. Considering that this chip is placed on the car's CAN network and many other identifiers are sent on this network, the amount of stimulation of receiving interruptions in the CAN network of this chip is very high, which causes interference in some functions. All received messages on CAN are of standard type, so they are 11-bit identifiers.&lt;BR /&gt;Please guide me about setting the best mask filters due to the required IDs for this chip in the processor expert section.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mizuz_0-1680860579382.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218223i3FC0905EFFA8DB58/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Mizuz_0-1680860579382.png" alt="Mizuz_0-1680860579382.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Mizuz_0-1680860579382.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;receives messages with the following identifiers:&lt;/P&gt;&lt;P&gt;0x082 -&amp;gt; 0000 1000 0010&lt;/P&gt;&lt;P&gt;0x088 -&amp;gt; 0000 1000 1000&lt;/P&gt;&lt;P&gt;0x094 -&amp;gt; 0000 1001 0100&lt;/P&gt;&lt;P&gt;0x0A2 -&amp;gt; 0000 1010 0010&lt;/P&gt;&lt;P&gt;0x0AE -&amp;gt; 0000 1010 1110&lt;/P&gt;&lt;P&gt;0x0A9 -&amp;gt; 0000 1010 1001&lt;/P&gt;&lt;P&gt;0x0C2 -&amp;gt; 0000 1100 0010&lt;/P&gt;&lt;P&gt;0x0E9 -&amp;gt; 0000 1110 1001&lt;/P&gt;&lt;P&gt;0x0E8 -&amp;gt; 0000 1110 1000&lt;/P&gt;&lt;P&gt;0x0C9 -&amp;gt; 0000 1100 1001&lt;/P&gt;&lt;P&gt;0x028 -&amp;gt; 0000 0010 1000&lt;/P&gt;&lt;P&gt;0x109 -&amp;gt; 0001 0000 1001&lt;/P&gt;&lt;P&gt;0x129 -&amp;gt; 0001 0010 1001&lt;/P&gt;&lt;P&gt;0x149 -&amp;gt; 0001 0100 1001&lt;/P&gt;&lt;P&gt;0x169 -&amp;gt; 0001 0110 1001&lt;/P&gt;&lt;P&gt;0x189 -&amp;gt; 0001 1000 1001&lt;/P&gt;&lt;P&gt;0x150 -&amp;gt; 0001 0101 0000&lt;/P&gt;&lt;P&gt;0x749 -&amp;gt; 0111 0100 1001&lt;/P&gt;&lt;P&gt;0x70A -&amp;gt; 0111 0000 1010&lt;/P&gt;&lt;P&gt;0x288 -&amp;gt; 0010 1000 1000&lt;/P&gt;&lt;P&gt;0x62C -&amp;gt; 0110 0010 1100&lt;/P&gt;&lt;P&gt;0x68C -&amp;gt; 0110 1000 1100&lt;/P&gt;&lt;P&gt;0x6AC -&amp;gt; 0110 1010 1100&lt;/P&gt;</description>
    <pubDate>Fri, 07 Apr 2023 09:45:41 GMT</pubDate>
    <dc:creator>Mizuz</dc:creator>
    <dc:date>2023-04-07T09:45:41Z</dc:date>
    <item>
      <title>Acceptance Mask MC9S08DZ96MLH</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Acceptance-Mask-MC9S08DZ96MLH/m-p/1629694#M23698</link>
      <description>&lt;P&gt;Hi, I am using the MC9S08DZ96MLH chip in a project. In this project, this chip receives messages with the following identifiers. Considering that this chip is placed on the car's CAN network and many other identifiers are sent on this network, the amount of stimulation of receiving interruptions in the CAN network of this chip is very high, which causes interference in some functions. All received messages on CAN are of standard type, so they are 11-bit identifiers.&lt;BR /&gt;Please guide me about setting the best mask filters due to the required IDs for this chip in the processor expert section.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Mizuz_0-1680860579382.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218223i3FC0905EFFA8DB58/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Mizuz_0-1680860579382.png" alt="Mizuz_0-1680860579382.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Mizuz_0-1680860579382.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;receives messages with the following identifiers:&lt;/P&gt;&lt;P&gt;0x082 -&amp;gt; 0000 1000 0010&lt;/P&gt;&lt;P&gt;0x088 -&amp;gt; 0000 1000 1000&lt;/P&gt;&lt;P&gt;0x094 -&amp;gt; 0000 1001 0100&lt;/P&gt;&lt;P&gt;0x0A2 -&amp;gt; 0000 1010 0010&lt;/P&gt;&lt;P&gt;0x0AE -&amp;gt; 0000 1010 1110&lt;/P&gt;&lt;P&gt;0x0A9 -&amp;gt; 0000 1010 1001&lt;/P&gt;&lt;P&gt;0x0C2 -&amp;gt; 0000 1100 0010&lt;/P&gt;&lt;P&gt;0x0E9 -&amp;gt; 0000 1110 1001&lt;/P&gt;&lt;P&gt;0x0E8 -&amp;gt; 0000 1110 1000&lt;/P&gt;&lt;P&gt;0x0C9 -&amp;gt; 0000 1100 1001&lt;/P&gt;&lt;P&gt;0x028 -&amp;gt; 0000 0010 1000&lt;/P&gt;&lt;P&gt;0x109 -&amp;gt; 0001 0000 1001&lt;/P&gt;&lt;P&gt;0x129 -&amp;gt; 0001 0010 1001&lt;/P&gt;&lt;P&gt;0x149 -&amp;gt; 0001 0100 1001&lt;/P&gt;&lt;P&gt;0x169 -&amp;gt; 0001 0110 1001&lt;/P&gt;&lt;P&gt;0x189 -&amp;gt; 0001 1000 1001&lt;/P&gt;&lt;P&gt;0x150 -&amp;gt; 0001 0101 0000&lt;/P&gt;&lt;P&gt;0x749 -&amp;gt; 0111 0100 1001&lt;/P&gt;&lt;P&gt;0x70A -&amp;gt; 0111 0000 1010&lt;/P&gt;&lt;P&gt;0x288 -&amp;gt; 0010 1000 1000&lt;/P&gt;&lt;P&gt;0x62C -&amp;gt; 0110 0010 1100&lt;/P&gt;&lt;P&gt;0x68C -&amp;gt; 0110 1000 1100&lt;/P&gt;&lt;P&gt;0x6AC -&amp;gt; 0110 1010 1100&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 09:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Acceptance-Mask-MC9S08DZ96MLH/m-p/1629694#M23698</guid>
      <dc:creator>Mizuz</dc:creator>
      <dc:date>2023-04-07T09:45:41Z</dc:date>
    </item>
  </channel>
</rss>