<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 9S08PL4 EEPROM in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-EEPROM/m-p/1617902#M23685</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to store one single byte to the EEPROM. As a test:&lt;/P&gt;&lt;P&gt;After checking if the first EEPROM byte contains 0xFF, I try to write it to 0x00.&lt;/P&gt;&lt;P&gt;FCLKDIV is OK,&lt;/P&gt;&lt;P&gt;CCIF is set,&lt;/P&gt;&lt;P&gt;ACCER and FPIVOL are both off,&lt;/P&gt;&lt;P&gt;FCCOBHI(0) ← 0x11 (EEPROM WRITE)&lt;/P&gt;&lt;P&gt;FCCOBLO(0) ← 0x80 (ADDRESS 23...16)&lt;/P&gt;&lt;P&gt;FCCOBHI(1) ← 0x31 (ADDRESS 15...8)&lt;/P&gt;&lt;P&gt;FCCOBLO(1) ← 0x00 (ADDRESS 7...0)&lt;/P&gt;&lt;P&gt;FCCOBLO(2) ← 0x00 (DESIRED CONTENT)&lt;/P&gt;&lt;P&gt;FSTAT ← 0x80 (START EXECUTION)&lt;/P&gt;&lt;P&gt;WAIT FOR CCIF SET&lt;/P&gt;&lt;P&gt;And then: ------ACCERR set!!!&lt;/P&gt;&lt;P&gt;The meaning can only be "command is not available in current mode".&lt;/P&gt;&lt;P&gt;It's only unavailable in unsecured mode, but I didn't use SD (secure device) on my CYCLONE programmer (from PE Micro).&lt;/P&gt;&lt;P&gt;What do I do after days of trying? I need to remember some values at next Power-up.&lt;/P&gt;&lt;P&gt;Pls help!&lt;/P&gt;</description>
    <pubDate>Fri, 17 Mar 2023 21:01:44 GMT</pubDate>
    <dc:creator>zebster</dc:creator>
    <dc:date>2023-03-17T21:01:44Z</dc:date>
    <item>
      <title>9S08PL4 EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-EEPROM/m-p/1617902#M23685</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to store one single byte to the EEPROM. As a test:&lt;/P&gt;&lt;P&gt;After checking if the first EEPROM byte contains 0xFF, I try to write it to 0x00.&lt;/P&gt;&lt;P&gt;FCLKDIV is OK,&lt;/P&gt;&lt;P&gt;CCIF is set,&lt;/P&gt;&lt;P&gt;ACCER and FPIVOL are both off,&lt;/P&gt;&lt;P&gt;FCCOBHI(0) ← 0x11 (EEPROM WRITE)&lt;/P&gt;&lt;P&gt;FCCOBLO(0) ← 0x80 (ADDRESS 23...16)&lt;/P&gt;&lt;P&gt;FCCOBHI(1) ← 0x31 (ADDRESS 15...8)&lt;/P&gt;&lt;P&gt;FCCOBLO(1) ← 0x00 (ADDRESS 7...0)&lt;/P&gt;&lt;P&gt;FCCOBLO(2) ← 0x00 (DESIRED CONTENT)&lt;/P&gt;&lt;P&gt;FSTAT ← 0x80 (START EXECUTION)&lt;/P&gt;&lt;P&gt;WAIT FOR CCIF SET&lt;/P&gt;&lt;P&gt;And then: ------ACCERR set!!!&lt;/P&gt;&lt;P&gt;The meaning can only be "command is not available in current mode".&lt;/P&gt;&lt;P&gt;It's only unavailable in unsecured mode, but I didn't use SD (secure device) on my CYCLONE programmer (from PE Micro).&lt;/P&gt;&lt;P&gt;What do I do after days of trying? I need to remember some values at next Power-up.&lt;/P&gt;&lt;P&gt;Pls help!&lt;/P&gt;</description>
      <pubDate>Fri, 17 Mar 2023 21:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-EEPROM/m-p/1617902#M23685</guid>
      <dc:creator>zebster</dc:creator>
      <dc:date>2023-03-17T21:01:44Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08PL4 EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-EEPROM/m-p/1618461#M23686</link>
      <description>&lt;P&gt;Never mind, it took one more weekend, but it's solved.&lt;/P&gt;&lt;P&gt;The Reference Manual is so bad I haven't seen anything like it.&lt;/P&gt;&lt;P&gt;Address 23, allegedly used to determine if it's FLASH or EEPROM, should be on FLASH setting (LO) to work with the EEPROM. Go figure.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Mar 2023 14:19:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-EEPROM/m-p/1618461#M23686</guid>
      <dc:creator>zebster</dc:creator>
      <dc:date>2023-03-20T14:19:51Z</dc:date>
    </item>
  </channel>
</rss>