<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックFree Master  Poll();</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Free-Master-Poll/m-p/1612951#M23681</link>
    <description>&lt;P&gt;Hi dears,&lt;/P&gt;&lt;P&gt;When i use&amp;nbsp;&lt;STRONG&gt;FMSTR_Poll();&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Dose FMSTR_Poll(); have to be executed twice to output correct results?&lt;/P&gt;&lt;P&gt;Well&amp;nbsp; i mean ,in the while(1)&amp;nbsp; &amp;nbsp;,the program have been executed once ,and the FMSTR_Poll() also&amp;nbsp; have been executed once. Will the value of the observation variable be transferred to the Freemaster ?&lt;/P&gt;&lt;P&gt;Because&amp;nbsp; when i was debugging the program i&amp;nbsp; found that ,for&amp;nbsp; the first time the&amp;nbsp; Poll&amp;nbsp; is&amp;nbsp; dealing with receiving data and decoding&amp;nbsp; and something, and the second time it will transmit data.&lt;/P&gt;</description>
    <pubDate>Fri, 10 Mar 2023 07:36:19 GMT</pubDate>
    <dc:creator>leang</dc:creator>
    <dc:date>2023-03-10T07:36:19Z</dc:date>
    <item>
      <title>Free Master  Poll();</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Free-Master-Poll/m-p/1612951#M23681</link>
      <description>&lt;P&gt;Hi dears,&lt;/P&gt;&lt;P&gt;When i use&amp;nbsp;&lt;STRONG&gt;FMSTR_Poll();&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Dose FMSTR_Poll(); have to be executed twice to output correct results?&lt;/P&gt;&lt;P&gt;Well&amp;nbsp; i mean ,in the while(1)&amp;nbsp; &amp;nbsp;,the program have been executed once ,and the FMSTR_Poll() also&amp;nbsp; have been executed once. Will the value of the observation variable be transferred to the Freemaster ?&lt;/P&gt;&lt;P&gt;Because&amp;nbsp; when i was debugging the program i&amp;nbsp; found that ,for&amp;nbsp; the first time the&amp;nbsp; Poll&amp;nbsp; is&amp;nbsp; dealing with receiving data and decoding&amp;nbsp; and something, and the second time it will transmit data.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Mar 2023 07:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Free-Master-Poll/m-p/1612951#M23681</guid>
      <dc:creator>leang</dc:creator>
      <dc:date>2023-03-10T07:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: Free Master  Poll();</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Free-Master-Poll/m-p/1614392#M23682</link>
      <description>&lt;P&gt;&amp;nbsp;Normally when you are using Free master you do not need to debug, please check the following application note&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN4752" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN4752&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Mar 2023 23:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Free-Master-Poll/m-p/1614392#M23682</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-03-13T23:44:13Z</dc:date>
    </item>
  </channel>
</rss>