<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1587229#M23630</link>
    <description>&lt;P&gt;Hello Quang,&lt;/P&gt;
&lt;P&gt;I hope all is great with you.&lt;/P&gt;
&lt;P&gt;This is because the trim coefficients are programmed by NXP between $FD40 and $FDFF.&lt;/P&gt;
&lt;P&gt;Writing the FLASH memory is done byte by byte, but erasing it is done page by page. In the NTM88, a page is 512-byte long and the full FLASH memory contains 16 pages. The trim coefficients are located in the page that starts at address $FC00 and ends at address $FDFF.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;I do not recommend to erase such values.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Tue, 24 Jan 2023 16:12:31 GMT</pubDate>
    <dc:creator>diazmarin09</dc:creator>
    <dc:date>2023-01-24T16:12:31Z</dc:date>
    <item>
      <title>memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration file</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1582742#M23624</link>
      <description>&lt;P&gt;Hi NXP support team.&lt;/P&gt;&lt;P&gt;I using Codewarrior Version: 11.1&lt;/P&gt;&lt;P&gt;NMT88 EV board.&lt;/P&gt;&lt;P&gt;Bootloader:&amp;nbsp; PE multilink&lt;/P&gt;&lt;P&gt;When i loading hex file i meet&amp;nbsp; codeWarrior Alert "&amp;nbsp;memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration file"&lt;/P&gt;&lt;P&gt;What does this mean&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="QuangCa_0-1673692421454.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/207357i8B4DD480C28EBCBD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="QuangCa_0-1673692421454.png" alt="QuangCa_0-1673692421454.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 14 Jan 2023 10:34:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1582742#M23624</guid>
      <dc:creator>QuangCa</dc:creator>
      <dc:date>2023-01-14T10:34:31Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1584178#M23625</link>
      <description>&lt;P&gt;&amp;nbsp;I am really sorry I did not get properly your question, can you please give me more information&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;also please tell us the part number that you are using&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 20:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1584178#M23625</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2023-01-17T20:43:01Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1586511#M23629</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Vicentegomez,&lt;/P&gt;&lt;P&gt;Sorry for my late reply, i am in vacation of new lunar year in Vietnam.&lt;/P&gt;&lt;P&gt;I mean when i flash the hex file in to &lt;SPAN&gt;NTM88H055&amp;nbsp;&lt;/SPAN&gt;IC,&lt;/P&gt;&lt;P&gt;I meet this alert&amp;nbsp;&amp;nbsp;"&amp;nbsp;memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration file"&lt;/P&gt;&lt;P&gt;So i worry about this alert make my code run fail.&lt;/P&gt;&lt;P&gt;But i check with this alert, my program run normal.&lt;/P&gt;&lt;P&gt;I don't know this alert for exactly what warning? Can you explain more for this alert?&lt;/P&gt;&lt;P&gt;thanks and best regards,&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 08:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1586511#M23629</guid>
      <dc:creator>QuangCa</dc:creator>
      <dc:date>2023-01-23T08:30:32Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1587229#M23630</link>
      <description>&lt;P&gt;Hello Quang,&lt;/P&gt;
&lt;P&gt;I hope all is great with you.&lt;/P&gt;
&lt;P&gt;This is because the trim coefficients are programmed by NXP between $FD40 and $FDFF.&lt;/P&gt;
&lt;P&gt;Writing the FLASH memory is done byte by byte, but erasing it is done page by page. In the NTM88, a page is 512-byte long and the full FLASH memory contains 16 pages. The trim coefficients are located in the page that starts at address $FC00 and ends at address $FDFF.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;I do not recommend to erase such values.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 16:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1587229#M23630</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-24T16:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1588302#M23633</link>
      <description>&lt;P&gt;Hi diazmarin09&lt;BR /&gt;So how can i need to do to pass this alert. Do i need re-configure for flash.&lt;BR /&gt;Sorry i am a new in NXP chipset.&lt;BR /&gt;I ignore this alert and my program is still run well.&lt;BR /&gt;thanks,&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 13:28:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1588302#M23633</guid>
      <dc:creator>QuangCa</dc:creator>
      <dc:date>2023-01-26T13:28:21Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1588437#M23634</link>
      <description>&lt;P&gt;Hello Quang,&lt;/P&gt;
&lt;P&gt;I am pleased to contact you again.&lt;/P&gt;
&lt;P&gt;In this case, I do recommend running an example project and use it as a reference for your design. It would be helpful if you reviewed the FLASH memory handling.&lt;/P&gt;
&lt;P&gt;Please let me know if you find the information above useful.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 17:19:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1588437#M23634</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-26T17:19:23Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1600143#M23658</link>
      <description>&lt;P&gt;I also encountered exactly same problem with example project from NXP, "NTM88_LocAngle_XZ".&lt;/P&gt;&lt;P&gt;This project contains data in FLASH of address 0xFD66 - 0xFDFF, the trim area.&lt;/P&gt;&lt;P&gt;Can we ignore these message?&lt;/P&gt;&lt;P&gt;This is map file of this project.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;Name                 Addr   hSize   dSize     Ref    Section   RLIB
---------------------------------------------------------------------
cau16BondwireLimits  FD66      10      16       0   .abs_section_fd66
cu16BondwireLimitXH  FD76       2       2       0   .abs_section_fd76
cu16BondwireLimitST  FD78       2       2       0   .abs_section_fd78
cu8SMISelfTestOff2   FD7E       1       1       0   .abs_section_fd7e
cu8SMISelfTestGain3  FD7F       1       1       0   .abs_section_fd7f

....

cu8Code1             FDFD       1       1       1   .abs_section_fdfd
cu8Code2             FDFE       1       1       1   .abs_section_fdfe
cu8Code3             FDFF       1       1       1   .abs_section_fdff
cu8FirmRel           FFAC       1       1       1   .abs_section_ffac
cu16TargetID         FFAD       2       2       0   .abs_section_ffad&lt;/LI-CODE&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="windy_0-1676516921294.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211145i3C5C9EE0F6F8A6A2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="windy_0-1676516921294.png" alt="windy_0-1676516921294.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Feb 2023 03:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1600143#M23658</guid>
      <dc:creator>windy</dc:creator>
      <dc:date>2023-02-16T03:15:44Z</dc:date>
    </item>
    <item>
      <title>Re: memory area from address 0xFD40 with size 2 is restricted for write in the memory configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1602154#M23663</link>
      <description>&lt;P&gt;Hello Windy,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope all is great with you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The following response has been validated with one of our specialists:&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Yes, it is normal. The warning informs the user that write and erase operations are prohibited on the trim page, in order not to erase or overwrite the trim coefficients.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;So, just click “Yes” and go ahead with the programming.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;In order not to see this message again, it is ok to tick “Remember my choice and don’t show this dialog”.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Please let me know if you find the information above useful.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 16:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/memory-area-from-address-0xFD40-with-size-2-is-restricted-for/m-p/1602154#M23663</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-02-20T16:50:35Z</dc:date>
    </item>
  </channel>
</rss>