<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックHow to set Filter and Mask in Controller Area Network (CAN bus) protocol?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-Filter-and-Mask-in-Controller-Area-Network-CAN-bus/m-p/1572517#M23613</link>
    <description>&lt;P&gt;Hi&lt;BR /&gt;I use IC mc9s08dz96. I want to use a mask and filter to receive CAN IDs. For this purpose, I have used the example in the &amp;nbsp;&lt;A href="https://images0.cnblogs.com/blog2015/268182/201508/100141563643661.png" target="_self"&gt;image&lt;/A&gt;&amp;nbsp;.&amp;nbsp;As it is known, The Transmitted ID is 01110101010(0x3AA), The Mask ID is 10100111000(0x538) and The filter ID is 00111101011(0x1EB). I use The CodeWarrior IDE, in CAN Properties, In Acceptance code 1 and&amp;nbsp;Acceptance code 2,I set&amp;nbsp;000001EB, In Acceptance Mask 1 ,&amp;nbsp;Acceptance Mask 2, I set&amp;nbsp;00000538. Then I send the&amp;nbsp;0x3AA from pc to MCU, But this ID is rejected.&lt;BR /&gt;When I send 0x00,&amp;nbsp;It is accepted.&amp;nbsp;Does anyone know where the problem is with my implementation?&lt;/P&gt;&lt;P&gt;I followed this example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205004i7E14F42A774E041E/image-size/medium?v=v2&amp;amp;px=400" alt="CAN1.png" title="CAN1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; This is my CAN properties:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FilterMaskSetting.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205005iC6D2F49B0EF940E2/image-size/medium?v=v2&amp;amp;px=400" alt="FilterMaskSetting.PNG" title="FilterMaskSetting.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And this is my transmitted ID:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="transmitCAN.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205006i8AAE5ED40CA55953/image-size/medium?v=v2&amp;amp;px=400" alt="transmitCAN.PNG" title="transmitCAN.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Dec 2022 11:59:37 GMT</pubDate>
    <dc:creator>mehdializadeh</dc:creator>
    <dc:date>2022-12-20T11:59:37Z</dc:date>
    <item>
      <title>How to set Filter and Mask in Controller Area Network (CAN bus) protocol?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-Filter-and-Mask-in-Controller-Area-Network-CAN-bus/m-p/1572517#M23613</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;I use IC mc9s08dz96. I want to use a mask and filter to receive CAN IDs. For this purpose, I have used the example in the &amp;nbsp;&lt;A href="https://images0.cnblogs.com/blog2015/268182/201508/100141563643661.png" target="_self"&gt;image&lt;/A&gt;&amp;nbsp;.&amp;nbsp;As it is known, The Transmitted ID is 01110101010(0x3AA), The Mask ID is 10100111000(0x538) and The filter ID is 00111101011(0x1EB). I use The CodeWarrior IDE, in CAN Properties, In Acceptance code 1 and&amp;nbsp;Acceptance code 2,I set&amp;nbsp;000001EB, In Acceptance Mask 1 ,&amp;nbsp;Acceptance Mask 2, I set&amp;nbsp;00000538. Then I send the&amp;nbsp;0x3AA from pc to MCU, But this ID is rejected.&lt;BR /&gt;When I send 0x00,&amp;nbsp;It is accepted.&amp;nbsp;Does anyone know where the problem is with my implementation?&lt;/P&gt;&lt;P&gt;I followed this example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205004i7E14F42A774E041E/image-size/medium?v=v2&amp;amp;px=400" alt="CAN1.png" title="CAN1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; This is my CAN properties:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FilterMaskSetting.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205005iC6D2F49B0EF940E2/image-size/medium?v=v2&amp;amp;px=400" alt="FilterMaskSetting.PNG" title="FilterMaskSetting.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And this is my transmitted ID:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="transmitCAN.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/205006i8AAE5ED40CA55953/image-size/medium?v=v2&amp;amp;px=400" alt="transmitCAN.PNG" title="transmitCAN.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 11:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-Filter-and-Mask-in-Controller-Area-Network-CAN-bus/m-p/1572517#M23613</guid>
      <dc:creator>mehdializadeh</dc:creator>
      <dc:date>2022-12-20T11:59:37Z</dc:date>
    </item>
    <item>
      <title>Re: How to set Filter and Mask in Controller Area Network (CAN bus) protocol?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-Filter-and-Mask-in-Controller-Area-Network-CAN-bus/m-p/1573233#M23616</link>
      <description>&lt;P&gt;&amp;nbsp;Sorry normally I do not use processor expert for CAN communication, I use the samples code under the&amp;nbsp;&lt;/P&gt;
&lt;H3 class="item-title"&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=MSCAN_S08&amp;amp;appType=license" target="_self"&gt;msCAN Driver for S08&lt;/A&gt;&lt;/H3&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also you can use the help on component for PE&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 21 Dec 2022 16:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-set-Filter-and-Mask-in-Controller-Area-Network-CAN-bus/m-p/1573233#M23616</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-12-21T16:40:58Z</dc:date>
    </item>
  </channel>
</rss>