<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Error when flashing program into NTM88 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Error-when-flashing-program-into-NTM88/m-p/1538103#M23572</link>
    <description>&lt;P&gt;When i flash program into NTM88, IDE (code warrior 11.1) throw out an error like picture attached. What are reason for this error and how can i fix it? thanks you so much. im using USB BDM&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 15 Oct 2022 14:15:36 GMT</pubDate>
    <dc:creator>nguyenhuy5997</dc:creator>
    <dc:date>2022-10-15T14:15:36Z</dc:date>
    <item>
      <title>Error when flashing program into NTM88</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Error-when-flashing-program-into-NTM88/m-p/1538103#M23572</link>
      <description>&lt;P&gt;When i flash program into NTM88, IDE (code warrior 11.1) throw out an error like picture attached. What are reason for this error and how can i fix it? thanks you so much. im using USB BDM&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 15 Oct 2022 14:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Error-when-flashing-program-into-NTM88/m-p/1538103#M23572</guid>
      <dc:creator>nguyenhuy5997</dc:creator>
      <dc:date>2022-10-15T14:15:36Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing program into NTM88</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Error-when-flashing-program-into-NTM88/m-p/1539034#M23573</link>
      <description>&lt;P&gt;Dear Huy,&lt;/P&gt;
&lt;P&gt;please refer to section 3.1 in the AN12523 attached. Part of the firmware flash is protected and cannot be overwritten.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1666077196649.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/197031i76EFBF8C26CA9281/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1666077196649.png" alt="JozefKozon_0-1666077196649.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please also refer to the AN13321 in the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13321.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13321.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 07:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Error-when-flashing-program-into-NTM88/m-p/1539034#M23573</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2022-10-18T07:15:02Z</dc:date>
    </item>
  </channel>
</rss>