<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックConfiguring a 68HC11F1</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuring-a-68HC11F1/m-p/1495701#M23549</link>
    <description>&lt;P&gt;So I have a project that uses a 68HC11F1, and I am not sure I have it set up correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Memory map (addresses not listed are not used):&lt;/P&gt;&lt;P&gt;0x0080-0x01FF Internal RAM (allocated for firmware use)&lt;/P&gt;&lt;P&gt;0x03D0-0x03FF Internal RAM (processor stack)&lt;/P&gt;&lt;P&gt;0x1000-0x105F HC11 register space (to be configured)&lt;/P&gt;&lt;P&gt;0x2000-0x200F I/O space 1&lt;/P&gt;&lt;P&gt;0x4000-0x400F I/O space 2&lt;/P&gt;&lt;P&gt;0xE000-0xFFBF Firmware ROM (external, 2764)&lt;/P&gt;&lt;P&gt;0xFFC0-0xFFFF Vectors (only XIRQ and Reset are required)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hardware configuration: Expanded mode (MODA, MODB pulled to +5V)&lt;/P&gt;&lt;P&gt;Port A, Port D, Port E, Port G: Not used&lt;/P&gt;&lt;P&gt;Port B: Address A8-A15&lt;/P&gt;&lt;P&gt;Port C: Data D0-D7&lt;/P&gt;&lt;P&gt;Port F: Address A0-A7&lt;/P&gt;&lt;P&gt;XTAL driven by external 1MHz&lt;/P&gt;&lt;P&gt;EXTAL pulled down w/ 10K resistor&lt;/P&gt;&lt;P&gt;E not connected&lt;/P&gt;&lt;P&gt;4XOUT: Not connected&lt;/P&gt;&lt;P&gt;IRQ: Pulled high&lt;/P&gt;&lt;P&gt;XIRQ: Driven by external signal&lt;/P&gt;&lt;P&gt;Vrh, Vrl: Pulled down w/ 10K resistor&lt;/P&gt;&lt;P&gt;R/W: Connected to other ICs as expected&lt;/P&gt;&lt;P&gt;Reset: Connected to other ICs as expected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, my question: Which registers in the group 0x1000-0x105F do I need to pay attention to?&lt;/P&gt;</description>
    <pubDate>Tue, 26 Jul 2022 16:03:04 GMT</pubDate>
    <dc:creator>meterman1980</dc:creator>
    <dc:date>2022-07-26T16:03:04Z</dc:date>
    <item>
      <title>Configuring a 68HC11F1</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuring-a-68HC11F1/m-p/1495701#M23549</link>
      <description>&lt;P&gt;So I have a project that uses a 68HC11F1, and I am not sure I have it set up correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Memory map (addresses not listed are not used):&lt;/P&gt;&lt;P&gt;0x0080-0x01FF Internal RAM (allocated for firmware use)&lt;/P&gt;&lt;P&gt;0x03D0-0x03FF Internal RAM (processor stack)&lt;/P&gt;&lt;P&gt;0x1000-0x105F HC11 register space (to be configured)&lt;/P&gt;&lt;P&gt;0x2000-0x200F I/O space 1&lt;/P&gt;&lt;P&gt;0x4000-0x400F I/O space 2&lt;/P&gt;&lt;P&gt;0xE000-0xFFBF Firmware ROM (external, 2764)&lt;/P&gt;&lt;P&gt;0xFFC0-0xFFFF Vectors (only XIRQ and Reset are required)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hardware configuration: Expanded mode (MODA, MODB pulled to +5V)&lt;/P&gt;&lt;P&gt;Port A, Port D, Port E, Port G: Not used&lt;/P&gt;&lt;P&gt;Port B: Address A8-A15&lt;/P&gt;&lt;P&gt;Port C: Data D0-D7&lt;/P&gt;&lt;P&gt;Port F: Address A0-A7&lt;/P&gt;&lt;P&gt;XTAL driven by external 1MHz&lt;/P&gt;&lt;P&gt;EXTAL pulled down w/ 10K resistor&lt;/P&gt;&lt;P&gt;E not connected&lt;/P&gt;&lt;P&gt;4XOUT: Not connected&lt;/P&gt;&lt;P&gt;IRQ: Pulled high&lt;/P&gt;&lt;P&gt;XIRQ: Driven by external signal&lt;/P&gt;&lt;P&gt;Vrh, Vrl: Pulled down w/ 10K resistor&lt;/P&gt;&lt;P&gt;R/W: Connected to other ICs as expected&lt;/P&gt;&lt;P&gt;Reset: Connected to other ICs as expected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, my question: Which registers in the group 0x1000-0x105F do I need to pay attention to?&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 16:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuring-a-68HC11F1/m-p/1495701#M23549</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2022-07-26T16:03:04Z</dc:date>
    </item>
  </channel>
</rss>