<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMCU bootloader dropped</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1470372#M23532</link>
    <description>&lt;P&gt;Dear:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN class=""&gt;Using NXP S9S08DZ60F2MLH to design a BCM, the project has been mass produced.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Product software using Bootloader+ applications.&lt;/SPAN&gt;&lt;SPAN class=""&gt; All functions of the product are normal when it leaves the factory, but all functions of the product are invalid after the customer uses it.&lt;/SPAN&gt;&lt;SPAN class=""&gt; After receiving the faulty prototype, perform the following tests: 1. The bootloader connection program fails to connect to the device; 2.&lt;/SPAN&gt;&lt;SPAN class=""&gt; 2. The running indicator light of the single chip is off;&lt;/SPAN&gt;&lt;SPAN class=""&gt; 3. The test crystal has no waveform output, and the test phenomenon is the same after replacement;&lt;/SPAN&gt;&lt;SPAN class=""&gt; 4. After the bootloader is rewritten, the connection is normal. After the application is upgraded, the product functions are restored. &lt;SPAN&gt;May I ask the possible cause of this problem?&amp;nbsp;&lt;/SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Jun 2022 05:44:05 GMT</pubDate>
    <dc:creator>jack_huang1</dc:creator>
    <dc:date>2022-06-08T05:44:05Z</dc:date>
    <item>
      <title>MCU bootloader dropped</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1470372#M23532</link>
      <description>&lt;P&gt;Dear:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN class=""&gt;Using NXP S9S08DZ60F2MLH to design a BCM, the project has been mass produced.&lt;/SPAN&gt;&lt;SPAN class=""&gt; Product software using Bootloader+ applications.&lt;/SPAN&gt;&lt;SPAN class=""&gt; All functions of the product are normal when it leaves the factory, but all functions of the product are invalid after the customer uses it.&lt;/SPAN&gt;&lt;SPAN class=""&gt; After receiving the faulty prototype, perform the following tests: 1. The bootloader connection program fails to connect to the device; 2.&lt;/SPAN&gt;&lt;SPAN class=""&gt; 2. The running indicator light of the single chip is off;&lt;/SPAN&gt;&lt;SPAN class=""&gt; 3. The test crystal has no waveform output, and the test phenomenon is the same after replacement;&lt;/SPAN&gt;&lt;SPAN class=""&gt; 4. After the bootloader is rewritten, the connection is normal. After the application is upgraded, the product functions are restored. &lt;SPAN&gt;May I ask the possible cause of this problem?&amp;nbsp;&lt;/SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 05:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1470372#M23532</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2022-06-08T05:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: MCU bootloader dropped</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1472404#M23533</link>
      <description>&lt;P&gt;Probably your code was corrupted maybe by EMI/ESD.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Maybe the device was turned off when it was writing to the flash this can cause damage.&lt;/P&gt;
&lt;P&gt;I recommend that you try to reproduce the problem in your facility. With this, you can decide the improvement that you can implement on your design.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There are some application notes about EMI and ESD on the nxp web page that can be helpful&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Vicente&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 20:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1472404#M23533</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-06-10T20:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCU bootloader dropped</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1474646#M23535</link>
      <description>&lt;P&gt;Ok, I will check it, but also I will delete it, because this is on the public community&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 17:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1474646#M23535</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-06-15T17:53:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCU bootloader dropped</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1475507#M23536</link>
      <description>&lt;P&gt;&amp;nbsp;I check the part of the schematics and it looks ok&lt;/P&gt;
&lt;P&gt;Please let me know if you have more information&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;have a good day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 18:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-bootloader-dropped/m-p/1475507#M23536</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-06-16T18:38:07Z</dc:date>
    </item>
  </channel>
</rss>