<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MMA7260Q - sleep mode</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130195#M2353</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;According to the data sheet, there are apparently built-in pull-down resistors on the g-select inputs, but nothing internally on the sleep mode pin.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Note that the active state of this pin is hign, so the use of an external pull-down resistor (rather than pull-up)&amp;nbsp;would give lower current in sleep mode.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Apr 2007 12:17:31 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2007-04-11T12:17:31Z</dc:date>
    <item>
      <title>MMA7260Q - sleep mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130194#M2352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Sorry for asking a non-mcu question here, but does anyone know if the MMA7260Q accelerometer has a built in pull-up on the /sleepmode pin?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I know I can just pull it up, but do I have to?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;uCTechnoGeek&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2007 07:36:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130194#M2352</guid>
      <dc:creator>UcTechnoGeek</dc:creator>
      <dc:date>2007-04-11T07:36:38Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7260Q - sleep mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130195#M2353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;According to the data sheet, there are apparently built-in pull-down resistors on the g-select inputs, but nothing internally on the sleep mode pin.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Note that the active state of this pin is hign, so the use of an external pull-down resistor (rather than pull-up)&amp;nbsp;would give lower current in sleep mode.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2007 12:17:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130195#M2353</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-04-11T12:17:31Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7260Q - sleep mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130196#M2354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My question is about MMA7260q hardware too, I was reading its datasheet&amp;nbsp; and I have connected mma6270q as indicated by the datasheet&amp;nbsp; but I can't get the right values when x es (+1g) -&amp;gt;2.45v or close to it I only got 1.8-1.9v and when x(-1g) I got 1.4v and is the same in y and z axis&amp;nbsp; why?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope&amp;nbsp; you can help me&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Sep 2010 09:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130196#M2354</guid>
      <dc:creator>Mayu</dc:creator>
      <dc:date>2010-09-28T09:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7260Q - sleep mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130197#M2355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To achieve a +1g voltage of 2.45 volt would require that the device be set to the highest sensitivity of 800 mV/g.&amp;nbsp; It appears that you may currently have the lowest sensitivity setting of 200 mV/g.&amp;nbsp; The nominal output would be 1.85 volt for +1g, and 1.45 volt for -1g, with this setting.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Oct 2010 11:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260Q-sleep-mode/m-p/130197#M2355</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-10-03T11:51:59Z</dc:date>
    </item>
  </channel>
</rss>