<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NCF29A1 motion detect pin configuration in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/NCF29A1-motion-detect-pin-configuration/m-p/1455773#M23507</link>
    <description>&lt;P&gt;Hello，I am using P21_MD of NCF29A1 as motion detect. but I find a problem that&amp;nbsp;&lt;SPAN&gt;when the motion sensor works, a high level pulse will be triggered, which will cause a large increase in power consumption. (Normal standby power consumption is 19uA, motion sensor operating power consumption is 400uA)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;At this time, the power consumption is not consumed by the motion sensor, because when I disconnect the resistance of&lt;/SPAN&gt;&lt;SPAN&gt; MU1R7, the overall power consumption will not increase when the motion sensor works, so it should be caused by the port of P21_MD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How should I configure the ports of P21_MD and software in this part to ensure that the power consumption of the ports will not be too high when the motion sensor works? &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 10 May 2022 14:35:28 GMT</pubDate>
    <dc:creator>Eternal</dc:creator>
    <dc:date>2022-05-10T14:35:28Z</dc:date>
    <item>
      <title>NCF29A1 motion detect pin configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/NCF29A1-motion-detect-pin-configuration/m-p/1455773#M23507</link>
      <description>&lt;P&gt;Hello，I am using P21_MD of NCF29A1 as motion detect. but I find a problem that&amp;nbsp;&lt;SPAN&gt;when the motion sensor works, a high level pulse will be triggered, which will cause a large increase in power consumption. (Normal standby power consumption is 19uA, motion sensor operating power consumption is 400uA)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;At this time, the power consumption is not consumed by the motion sensor, because when I disconnect the resistance of&lt;/SPAN&gt;&lt;SPAN&gt; MU1R7, the overall power consumption will not increase when the motion sensor works, so it should be caused by the port of P21_MD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How should I configure the ports of P21_MD and software in this part to ensure that the power consumption of the ports will not be too high when the motion sensor works? &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 May 2022 14:35:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/NCF29A1-motion-detect-pin-configuration/m-p/1455773#M23507</guid>
      <dc:creator>Eternal</dc:creator>
      <dc:date>2022-05-10T14:35:28Z</dc:date>
    </item>
    <item>
      <title>Re: NCF29A1 motion detect pin configuration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/NCF29A1-motion-detect-pin-configuration/m-p/1456707#M23508</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the NCF family is part of the&lt;SPAN&gt;&amp;nbsp;Keyless product, you need to contact your local sales to get support for this device.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Vicente&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 May 2022 21:09:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/NCF29A1-motion-detect-pin-configuration/m-p/1456707#M23508</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-05-11T21:09:31Z</dc:date>
    </item>
  </channel>
</rss>