<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックThe Classification and Application of Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-Classification-and-Application-of-Microcontrollers/m-p/1441580#M23499</link>
    <description>&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.apogeeweb.net/electron/popularization-of-science-mcu.html" target="_self"&gt;&lt;STRONG&gt;Microcontrollers &lt;/STRONG&gt;&lt;/A&gt;are classified into two types based on their memory type: those with no on-chip ROM&amp;nbsp; and those with on-chip ROM,&amp;nbsp; The chip without on-chip ROM&amp;nbsp; must be used externally with EPROM&amp;nbsp;(typically 8031); the chip with on-chip ROM&amp;nbsp; is classified as on-chip EPROM (typically 87C51), MASK on-chip mask&amp;nbsp;ROM&amp;nbsp; (typically 8051), on-chip Flash (typically 89C51), and other types.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;MCUs are classified into two types based on their intended use: general-purpose and special-purpose. It is classified into4,&amp;nbsp;8, 16, and 32-bit MCUs based on the width of the data bus and the number of data bytes that can be processed at the same time.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 09 Apr 2022 08:43:20 GMT</pubDate>
    <dc:creator>xiaoye</dc:creator>
    <dc:date>2022-04-09T08:43:20Z</dc:date>
    <item>
      <title>The Classification and Application of Microcontrollers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-Classification-and-Application-of-Microcontrollers/m-p/1441580#M23499</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.apogeeweb.net/electron/popularization-of-science-mcu.html" target="_self"&gt;&lt;STRONG&gt;Microcontrollers &lt;/STRONG&gt;&lt;/A&gt;are classified into two types based on their memory type: those with no on-chip ROM&amp;nbsp; and those with on-chip ROM,&amp;nbsp; The chip without on-chip ROM&amp;nbsp; must be used externally with EPROM&amp;nbsp;(typically 8031); the chip with on-chip ROM&amp;nbsp; is classified as on-chip EPROM (typically 87C51), MASK on-chip mask&amp;nbsp;ROM&amp;nbsp; (typically 8051), on-chip Flash (typically 89C51), and other types.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;MCUs are classified into two types based on their intended use: general-purpose and special-purpose. It is classified into4,&amp;nbsp;8, 16, and 32-bit MCUs based on the width of the data bus and the number of data bytes that can be processed at the same time.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 09 Apr 2022 08:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/The-Classification-and-Application-of-Microcontrollers/m-p/1441580#M23499</guid>
      <dc:creator>xiaoye</dc:creator>
      <dc:date>2022-04-09T08:43:20Z</dc:date>
    </item>
  </channel>
</rss>