<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08AC60 will not load data from EEPROM in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417108#M23482</link>
    <description>&lt;P&gt;Can you please give me more information about the problem: After the micro processes an IRQ there is no MOSI/MISO data activity.&lt;/P&gt;&lt;P&gt;Are you using an external EEPROM: Yes after the Micro IRQ the data from the Micro is loaded to the EEPROM through a level shifter to a graphic display. Problem is the graphic data is not displayed from the Micro.&lt;/P&gt;&lt;P&gt;Are you using SPI or llC to load the data on the EEPROM: I Sam using SPI MOSI/MISO to load the EEPROM&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Feb 2022 02:58:35 GMT</pubDate>
    <dc:creator>wtyler</dc:creator>
    <dc:date>2022-02-22T02:58:35Z</dc:date>
    <item>
      <title>MC9S08AC60 will not load data from EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1413287#M23478</link>
      <description>&lt;P&gt;I am currently using a&amp;nbsp;MC9S08AC60 to control a Key Pad and display. The problem is after a while the Micro will not load the the 4KB EEPROM graphics data to the display after a KBI1P4/PTG4 is triggered.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 23:03:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1413287#M23478</guid>
      <dc:creator>wtyler</dc:creator>
      <dc:date>2022-02-14T23:03:01Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08AC60 will not load data from EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1414930#M23479</link>
      <description>&lt;P&gt;can you please give me more information about the problem&lt;/P&gt;
&lt;P&gt;are you using an external eeprom?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;are you using SPI or IIC to load the data on the EEPROM?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Thu, 17 Feb 2022 03:07:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1414930#M23479</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-02-17T03:07:19Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08AC60 will not load data from EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417108#M23482</link>
      <description>&lt;P&gt;Can you please give me more information about the problem: After the micro processes an IRQ there is no MOSI/MISO data activity.&lt;/P&gt;&lt;P&gt;Are you using an external EEPROM: Yes after the Micro IRQ the data from the Micro is loaded to the EEPROM through a level shifter to a graphic display. Problem is the graphic data is not displayed from the Micro.&lt;/P&gt;&lt;P&gt;Are you using SPI or llC to load the data on the EEPROM: I Sam using SPI MOSI/MISO to load the EEPROM&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 02:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417108#M23482</guid>
      <dc:creator>wtyler</dc:creator>
      <dc:date>2022-02-22T02:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08AC60 will not load data from EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417465#M23483</link>
      <description>&lt;P&gt;Can you check if the data is sending properly on the SPI to the EEPROM?&lt;/P&gt;
&lt;P&gt;Do you have any flag pending?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;have a good day&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 12:06:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417465#M23483</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2022-02-22T12:06:25Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08AC60 will not load data from EEPROM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417708#M23484</link>
      <description>&lt;P&gt;After the IRQ no data is sent to the EEPROM. I don’t know how to check the flags.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 19:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08AC60-will-not-load-data-from-EEPROM/m-p/1417708#M23484</guid>
      <dc:creator>wtyler</dc:creator>
      <dc:date>2022-02-22T19:55:54Z</dc:date>
    </item>
  </channel>
</rss>