<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 M9S08QG8 development board</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08QG8-development-board/m-p/1353714#M23415</link>
    <description>&lt;P&gt;Hi People.&lt;/P&gt;&lt;P&gt;Currently I want to use the demo board DEMO9S08QG8 from&amp;nbsp; development board, I use IDE Codewarrior V 6.3 with no problem with FL16 Microcontroller, and others boards, however this board has no communication with my codewarrior.&lt;/P&gt;&lt;P&gt;I could discover that this demo board DEMO9S08QG8 is under "Multilink USB 2.0" in the devices config list whn I connect it to my computer through and USB cable, so I believe there is a misunderstanding between the DEMO9S08QG8 board and my Windows 10 because of wrong assigned drivers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help me with the proper drivers for the DEMO9S08QG8 board, or maybe you can show me another flash prgramming board, as I have developed my application already, What I need is to load the s19 file into the flash of microcontroller.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Mon, 11 Oct 2021 20:30:33 GMT</pubDate>
    <dc:creator>miguelangelferr</dc:creator>
    <dc:date>2021-10-11T20:30:33Z</dc:date>
    <item>
      <title>M9S08QG8 development board</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08QG8-development-board/m-p/1353714#M23415</link>
      <description>&lt;P&gt;Hi People.&lt;/P&gt;&lt;P&gt;Currently I want to use the demo board DEMO9S08QG8 from&amp;nbsp; development board, I use IDE Codewarrior V 6.3 with no problem with FL16 Microcontroller, and others boards, however this board has no communication with my codewarrior.&lt;/P&gt;&lt;P&gt;I could discover that this demo board DEMO9S08QG8 is under "Multilink USB 2.0" in the devices config list whn I connect it to my computer through and USB cable, so I believe there is a misunderstanding between the DEMO9S08QG8 board and my Windows 10 because of wrong assigned drivers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you help me with the proper drivers for the DEMO9S08QG8 board, or maybe you can show me another flash prgramming board, as I have developed my application already, What I need is to load the s19 file into the flash of microcontroller.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 11 Oct 2021 20:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08QG8-development-board/m-p/1353714#M23415</guid>
      <dc:creator>miguelangelferr</dc:creator>
      <dc:date>2021-10-11T20:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: M9S08QG8 development board</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08QG8-development-board/m-p/1355371#M23416</link>
      <description>&lt;P&gt;We do not recomment to use codewarrior 6.3 any more, this is no longer supported, I recommend you that change to codewarrior 11.1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also can you try to use the tools from P&amp;amp;E and the end the&amp;nbsp;&lt;SPAN&gt;DEMO9S08QG8 has a OSBM on it&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/osbdm/" target="_blank"&gt;https://www.pemicro.com/osbdm/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;Vicente&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Oct 2021 23:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08QG8-development-board/m-p/1355371#M23416</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-10-13T23:08:44Z</dc:date>
    </item>
  </channel>
</rss>