<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS08DZ60 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60/m-p/1337872#M23407</link>
    <description>&lt;P&gt;The only difference that this pin has is&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The PTE1 pin does not contain a clamp diode to VDD and should not be&lt;BR /&gt;driven above VDD. The voltage measured on the internally pulled up&lt;BR /&gt;PTE1 pin may be as low as VDD – 0.7 V. The internal gates connected&lt;BR /&gt;to this pin are pulled all the way to VDD&lt;/P&gt;
&lt;P&gt;But this does not affect the programming or the memory&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Vicente G&lt;/P&gt;</description>
    <pubDate>Thu, 09 Sep 2021 18:10:26 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2021-09-09T18:10:26Z</dc:date>
    <item>
      <title>HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60/m-p/1337678#M23406</link>
      <description>&lt;P&gt;I'm working with S9S08DZ32F2MLC, 32 pin, 32K flash.&lt;/P&gt;&lt;P&gt;SOMEONE CAN EXPLAIN IF THERE IS A CORRELATION BETWEEN THE PROGRAMMING OF THE FLASH AND THE EEPROM AND THE PTE1 PIN?&lt;BR /&gt;ON SOME PIECES WITH PTE1 = 0 THE EPROM IS NOT PROGRAMMED AND NOT EVEN THE FLASH&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 10:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60/m-p/1337678#M23406</guid>
      <dc:creator>BOLFRA</dc:creator>
      <dc:date>2021-09-09T10:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60/m-p/1337872#M23407</link>
      <description>&lt;P&gt;The only difference that this pin has is&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The PTE1 pin does not contain a clamp diode to VDD and should not be&lt;BR /&gt;driven above VDD. The voltage measured on the internally pulled up&lt;BR /&gt;PTE1 pin may be as low as VDD – 0.7 V. The internal gates connected&lt;BR /&gt;to this pin are pulled all the way to VDD&lt;/P&gt;
&lt;P&gt;But this does not affect the programming or the memory&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Vicente G&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 18:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08DZ60/m-p/1337872#M23407</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-09-09T18:10:26Z</dc:date>
    </item>
  </channel>
</rss>