<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debugger &amp;amp; flash programmer in CW 10.4 for HCS08: different result in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1322027#M23404</link>
    <description>&lt;P&gt;Can you give me a little bit more details?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is with any project or only with a specific one?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Aug 2021 17:19:04 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2021-08-11T17:19:04Z</dc:date>
    <item>
      <title>Debugger &amp; flash programmer in CW 10.4 for HCS08: different result</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1321313#M23403</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;everything is working fine when the target is programmed using the debugger but as soon as the flash programmer is used, the target is no more booting.&lt;/P&gt;&lt;P&gt;We disabled all checksum, remove the watchdog but no result.&lt;/P&gt;&lt;P&gt;We are using PE Mircom USB Multilink and also the newer one; same result.&lt;/P&gt;&lt;P&gt;We also tried with CW 6.2 and same result too with the flash programmer.&lt;/P&gt;&lt;P&gt;Any hint on what to look next ?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Aug 2021 20:11:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1321313#M23403</guid>
      <dc:creator>damorin</dc:creator>
      <dc:date>2021-08-10T20:11:08Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger &amp; flash programmer in CW 10.4 for HCS08: different result</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1322027#M23404</link>
      <description>&lt;P&gt;Can you give me a little bit more details?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;this is with any project or only with a specific one?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 17:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1322027#M23404</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-08-11T17:19:04Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger &amp; flash programmer in CW 10.4 for HCS08: different result</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1322114#M23405</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;now it's working; it was two problems from two different sources (wrong CW version and a bug in the code).&lt;/P&gt;&lt;P&gt;Happy to say 'not a bug'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Aug 2021 19:40:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Debugger-amp-flash-programmer-in-CW-10-4-for-HCS08-different/m-p/1322114#M23405</guid>
      <dc:creator>damorin</dc:creator>
      <dc:date>2021-08-11T19:40:53Z</dc:date>
    </item>
  </channel>
</rss>