<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Which 68HC11 version? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1260658#M23337</link>
    <description>&lt;P&gt;No, sorry, it does not use the same opcodes&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 12 Apr 2021 15:14:06 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2021-04-12T15:14:06Z</dc:date>
    <item>
      <title>Which 68HC11 version?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1253156#M23330</link>
      <description>&lt;P&gt;Some time ago, I posted a question asking about the Motorola SC44125P CPU, and I eventually determined that it is a custom 6800 with pre-programmed, dedicated data bus (8 bit) and address bus (16 bit) pins, along with the 6801 instruction set. Although it has the option, neither the on-board RAM or ROM are used.&lt;/P&gt;&lt;P&gt;After some brief comparison of later 68xx CPUs, I see the 68HC11 comes closest, but want to know which would be a suitable version (or newer replacement) that would work the best.&lt;/P&gt;&lt;P&gt;Requirements:&lt;/P&gt;&lt;P&gt;6801 or 68HC11 instruction set&lt;BR /&gt;Ability to disable on-board RAM / ROM&lt;BR /&gt;Dedicated 16-bit address bus pins or the ability to easily program same&lt;BR /&gt;Dedicated 8-bit data bus pins or ability to program same&lt;BR /&gt;Support pins required: R/~W, Clock input (1MHz), ~IRQ, ~IRQ2, ~NMI, and ~Reset&lt;/P&gt;</description>
      <pubDate>Sat, 27 Mar 2021 17:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1253156#M23330</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2021-03-27T17:49:14Z</dc:date>
    </item>
    <item>
      <title>Re: Which 68HC11 version?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1254397#M23331</link>
      <description>&lt;P&gt;Sorry all the HC11 is obsoleted&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So I can not recommend you any HC11 device.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you want you can move to the S08 family like the mc9s08pb family&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit-s08-mcus/8-bit-5v-full-featured-mcu-with-rich-analog:S08PB" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit-s08-mcus/8-bit-5v-full-featured-mcu-with-rich-analog:S08PB&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this will help you&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Mar 2021 17:19:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1254397#M23331</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-03-30T17:19:51Z</dc:date>
    </item>
    <item>
      <title>Re: Which 68HC11 version?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1260017#M23336</link>
      <description>&lt;P&gt;Does it use the same opcodes as the MC6801?&lt;/P&gt;&lt;P&gt;I'm hoping to see if there's anything I can use without having to rewrite 16K of densely written assembly.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Apr 2021 00:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1260017#M23336</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2021-04-11T00:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: Which 68HC11 version?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1260658#M23337</link>
      <description>&lt;P&gt;No, sorry, it does not use the same opcodes&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Apr 2021 15:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1260658#M23337</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-04-12T15:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: Which 68HC11 version?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1282897#M23358</link>
      <description>&lt;P&gt;If you're attached to HC11 assembly code, maybe you could use a 9S12 to upgrade your design. At those ancient times it was said it was assembly source compatible, although object code was not compatible at all. You could check AN2708 which deals with External Bus Interface on the HCS12X.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Celso&lt;/P&gt;</description>
      <pubDate>Wed, 26 May 2021 21:20:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-68HC11-version/m-p/1282897#M23358</guid>
      <dc:creator>celsoken</dc:creator>
      <dc:date>2021-05-26T21:20:58Z</dc:date>
    </item>
  </channel>
</rss>