<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can the MC9S08SG8 output the clock? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249117#M23325</link>
    <description>&lt;P&gt;The SG family does not have a clock out pin, if you want to get the 32KHz from the internal clock this is not possible, but you can use the internal FLL and the TPM module to get a PWM signal on one of the TPM channels, I&amp;nbsp; do not remember if this possible to have 32KHz using the TPM, please check the following code, this is for the SH, the SH has the same modules than the SG&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 20 Mar 2021 04:25:54 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2021-03-20T04:25:54Z</dc:date>
    <item>
      <title>Can the MC9S08SG8 output the clock?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1247865#M23323</link>
      <description>&lt;P&gt;Does anyone can tell me how to output the clock from the internal clock source of MC9S08SG8 ?&lt;/P&gt;&lt;P&gt;Which register should i use? I want know the detils.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 06:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1247865#M23323</guid>
      <dc:creator>Abner</dc:creator>
      <dc:date>2021-03-18T06:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: Can the MC9S08SG8 output the clock?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249117#M23325</link>
      <description>&lt;P&gt;The SG family does not have a clock out pin, if you want to get the 32KHz from the internal clock this is not possible, but you can use the internal FLL and the TPM module to get a PWM signal on one of the TPM channels, I&amp;nbsp; do not remember if this possible to have 32KHz using the TPM, please check the following code, this is for the SH, the SH has the same modules than the SG&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 20 Mar 2021 04:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249117#M23325</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-03-20T04:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can the MC9S08SG8 output the clock?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249236#M23328</link>
      <description>&lt;P&gt;Thanks for your reply!&lt;/P&gt;&lt;P&gt;In another way,I want to know can i output a signal like the follow picture on MC9S08SG8 PTA1 pin.&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="捕获.JPG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/140226i3596A6DAF5E34F5B/image-size/large?v=v2&amp;amp;px=999" role="button" title="捕获.JPG" alt="捕获.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 02:06:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249236#M23328</guid>
      <dc:creator>Abner</dc:creator>
      <dc:date>2021-03-22T02:06:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can the MC9S08SG8 output the clock?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249916#M23329</link>
      <description>&lt;P&gt;You only can have a PWM signal (square signal), not a clock signal (sine signal)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a good day&lt;/P&gt;</description>
      <pubDate>Mon, 22 Mar 2021 22:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-the-MC9S08SG8-output-the-clock/m-p/1249916#M23329</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-03-22T22:32:17Z</dc:date>
    </item>
  </channel>
</rss>