<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMultilink 2.0 Does not work wit CodeWarrior 10.7</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Multilink-2-0-Does-not-work-wit-CodeWarrior-10-7/m-p/1212759#M23256</link>
    <description>&lt;P&gt;Operating System: Windows 10 64-bit&lt;/P&gt;&lt;P&gt;I installed drivers for DEMO9S08QG8. Windriver and USB Multilink 2.0 appears&lt;BR /&gt;without problems, I mean Windows shows that device is working correctly.&lt;/P&gt;&lt;P&gt;When I tried to connect with Codewarrior 10.7 (at 2016 I can use the Demoboard&lt;BR /&gt;without troubles), the IDE cannot recognize the connection.&lt;/P&gt;&lt;P&gt;I download Update Firmware Multilink from P&amp;amp;E site and also not recognize the&lt;BR /&gt;connection.&lt;/P&gt;&lt;P&gt;I attached pdf files where I show you that happens with CW 10.7.&lt;/P&gt;&lt;P&gt;First I used the P&amp;amp;E drivers 12.7 (the last release), then I used the 12.3&lt;BR /&gt;version.&lt;/P&gt;&lt;P&gt;Installed CW 10.7 and P&amp;amp;E Drivers 12.3 with compatibility W8.&lt;/P&gt;&lt;P&gt;I used W10 at 64bits.&lt;/P&gt;&lt;P&gt;Also I attached a note at 2016, when I had troubles for prog. only is in&lt;BR /&gt;spanish because was only for me like a log.&lt;/P&gt;&lt;P&gt;I hope so you can help me.&lt;/P&gt;</description>
    <pubDate>Sat, 16 Jan 2021 15:21:10 GMT</pubDate>
    <dc:creator>monroy39</dc:creator>
    <dc:date>2021-01-16T15:21:10Z</dc:date>
    <item>
      <title>Multilink 2.0 Does not work wit CodeWarrior 10.7</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Multilink-2-0-Does-not-work-wit-CodeWarrior-10-7/m-p/1212759#M23256</link>
      <description>&lt;P&gt;Operating System: Windows 10 64-bit&lt;/P&gt;&lt;P&gt;I installed drivers for DEMO9S08QG8. Windriver and USB Multilink 2.0 appears&lt;BR /&gt;without problems, I mean Windows shows that device is working correctly.&lt;/P&gt;&lt;P&gt;When I tried to connect with Codewarrior 10.7 (at 2016 I can use the Demoboard&lt;BR /&gt;without troubles), the IDE cannot recognize the connection.&lt;/P&gt;&lt;P&gt;I download Update Firmware Multilink from P&amp;amp;E site and also not recognize the&lt;BR /&gt;connection.&lt;/P&gt;&lt;P&gt;I attached pdf files where I show you that happens with CW 10.7.&lt;/P&gt;&lt;P&gt;First I used the P&amp;amp;E drivers 12.7 (the last release), then I used the 12.3&lt;BR /&gt;version.&lt;/P&gt;&lt;P&gt;Installed CW 10.7 and P&amp;amp;E Drivers 12.3 with compatibility W8.&lt;/P&gt;&lt;P&gt;I used W10 at 64bits.&lt;/P&gt;&lt;P&gt;Also I attached a note at 2016, when I had troubles for prog. only is in&lt;BR /&gt;spanish because was only for me like a log.&lt;/P&gt;&lt;P&gt;I hope so you can help me.&lt;/P&gt;</description>
      <pubDate>Sat, 16 Jan 2021 15:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Multilink-2-0-Does-not-work-wit-CodeWarrior-10-7/m-p/1212759#M23256</guid>
      <dc:creator>monroy39</dc:creator>
      <dc:date>2021-01-16T15:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: Multilink 2.0 Does not work wit CodeWarrior 10.7</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Multilink-2-0-Does-not-work-wit-CodeWarrior-10-7/m-p/1217153#M23258</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What multilink are you using?&lt;/P&gt;
&lt;P&gt;depending the multilink that you have, in some version there are 2 led on in, one is for the multilink power, the second is on when the multilink detect the board (target)&lt;/P&gt;
&lt;P&gt;I have win 10&amp;nbsp; 64bit and the USB universal multilink is working without problems&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know your comments&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Vicente&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 22:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Multilink-2-0-Does-not-work-wit-CodeWarrior-10-7/m-p/1217153#M23258</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-01-19T22:50:45Z</dc:date>
    </item>
  </channel>
</rss>