<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックCan MC9S08AWCFGE MCU be programed with DEMO9S08AW60E demonstration board?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-MC9S08AWCFGE-MCU-be-programed-with-DEMO9S08AW60E/m-p/1184869#M23230</link>
    <description>&lt;P&gt;&lt;FONT face="Liberation Serif, serif"&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;Hi sir,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Liberation Serif, serif"&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;I am finding the demonstration board that can program the&amp;nbsp;MC9S08AW32CFGE microcontroller (44pin). I found that&amp;nbsp;MC9S08AW32CFGE is in the&amp;nbsp;MC9S08AW Family and the DEMO9S08AW60E is a demonstration board for the MC9S08AW60 (64pin) microcontroller that is in MC9S08AW Family too. So, I wonder that&amp;nbsp;DEMO9S08AW60E&amp;nbsp;demonstration board can be used for&amp;nbsp;MC9S08AW32CFGE MCU or not? If it can not use, please suggest&amp;nbsp;which&amp;nbsp;demonstration board that I can use for program my&amp;nbsp;MC9S08AW32CFGE MCU?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Liberation Serif, serif"&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;Thank you for your support&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 18 Nov 2020 03:32:57 GMT</pubDate>
    <dc:creator>parnravee</dc:creator>
    <dc:date>2020-11-18T03:32:57Z</dc:date>
    <item>
      <title>Can MC9S08AWCFGE MCU be programed with DEMO9S08AW60E demonstration board?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-MC9S08AWCFGE-MCU-be-programed-with-DEMO9S08AW60E/m-p/1184869#M23230</link>
      <description>&lt;P&gt;&lt;FONT face="Liberation Serif, serif"&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;Hi sir,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Liberation Serif, serif"&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;I am finding the demonstration board that can program the&amp;nbsp;MC9S08AW32CFGE microcontroller (44pin). I found that&amp;nbsp;MC9S08AW32CFGE is in the&amp;nbsp;MC9S08AW Family and the DEMO9S08AW60E is a demonstration board for the MC9S08AW60 (64pin) microcontroller that is in MC9S08AW Family too. So, I wonder that&amp;nbsp;DEMO9S08AW60E&amp;nbsp;demonstration board can be used for&amp;nbsp;MC9S08AW32CFGE MCU or not? If it can not use, please suggest&amp;nbsp;which&amp;nbsp;demonstration board that I can use for program my&amp;nbsp;MC9S08AW32CFGE MCU?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Liberation Serif, serif"&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;Thank you for your support&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Nov 2020 03:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-MC9S08AWCFGE-MCU-be-programed-with-DEMO9S08AW60E/m-p/1184869#M23230</guid>
      <dc:creator>parnravee</dc:creator>
      <dc:date>2020-11-18T03:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: Can MC9S08AWCFGE MCU be programed with DEMO9S08AW60E demonstration board?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-MC9S08AWCFGE-MCU-be-programed-with-DEMO9S08AW60E/m-p/1187730#M23232</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;you can use the demo board to program any S08, just you need to open the BKGD line and plug the new device (in this case the AW32 ) pins for programming (reset, VDD,GND, and&amp;nbsp; BKGD). These lines need to tied to the lines on the DEMO boards that came from the OSBDM ( in this board I am not sure if this is an S12 device or the S08JM) and you should be able to program the AW32.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You do not need the other pins to program this device.&lt;/P&gt;
&lt;P&gt;I hope this will help you&lt;/P&gt;
&lt;P&gt;Have a good day&lt;/P&gt;</description>
      <pubDate>Mon, 23 Nov 2020 22:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-MC9S08AWCFGE-MCU-be-programed-with-DEMO9S08AW60E/m-p/1187730#M23232</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-11-23T22:41:36Z</dc:date>
    </item>
  </channel>
</rss>