<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 9S08PL4 PTA4, PTA5 USED AS OUTPUT in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-PTA4-PTA5-USED-AS-OUTPUT/m-p/1182655#M23228</link>
    <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am new to this particular device and have a strange problem with it. All 6 PTA pins are used as outputs, the load is minimal, driving CMOS inputs.&lt;/P&gt;&lt;P&gt;My program starts and does what it should, on the other port pins, but these two turn HI and no matter what I do, they stay there.&lt;/P&gt;&lt;P&gt;I already won the battle with the WATCHDOG. Is there anything else overwriting these two out of POR?&lt;/P&gt;&lt;P&gt;Thanks for a possible quick answer&lt;/P&gt;&lt;P&gt;Laszlo&lt;/P&gt;</description>
    <pubDate>Fri, 13 Nov 2020 01:24:41 GMT</pubDate>
    <dc:creator>leslie</dc:creator>
    <dc:date>2020-11-13T01:24:41Z</dc:date>
    <item>
      <title>9S08PL4 PTA4, PTA5 USED AS OUTPUT</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-PTA4-PTA5-USED-AS-OUTPUT/m-p/1182655#M23228</link>
      <description>&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am new to this particular device and have a strange problem with it. All 6 PTA pins are used as outputs, the load is minimal, driving CMOS inputs.&lt;/P&gt;&lt;P&gt;My program starts and does what it should, on the other port pins, but these two turn HI and no matter what I do, they stay there.&lt;/P&gt;&lt;P&gt;I already won the battle with the WATCHDOG. Is there anything else overwriting these two out of POR?&lt;/P&gt;&lt;P&gt;Thanks for a possible quick answer&lt;/P&gt;&lt;P&gt;Laszlo&lt;/P&gt;</description>
      <pubDate>Fri, 13 Nov 2020 01:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-PTA4-PTA5-USED-AS-OUTPUT/m-p/1182655#M23228</guid>
      <dc:creator>leslie</dc:creator>
      <dc:date>2020-11-13T01:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08PL4 PTA4, PTA5 USED AS OUTPUT</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-PTA4-PTA5-USED-AS-OUTPUT/m-p/1183565#M23229</link>
      <description>&lt;P&gt;I got it running, "case closed". BKGD and RESET activated out of POR; had to disable. FUN...&lt;/P&gt;</description>
      <pubDate>Mon, 16 Nov 2020 03:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08PL4-PTA4-PTA5-USED-AS-OUTPUT/m-p/1183565#M23229</guid>
      <dc:creator>leslie</dc:creator>
      <dc:date>2020-11-16T03:34:12Z</dc:date>
    </item>
  </channel>
</rss>