<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Problem with AN3927 using JM60 in windows 10</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-AN3927-using-JM60-in-windows-10/m-p/1094500#M23191</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved the malformed packet problem with max get lun, but, i saw the scsi commands routines doesn't works. There isn't return with Inquiry command routine. How the microcontroller knows the variable who send the information to the host? I need to pointer to this variable and i don't know which is.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2020 12:28:37 GMT</pubDate>
    <dc:creator>eduardo1</dc:creator>
    <dc:date>2020-07-28T12:28:37Z</dc:date>
    <item>
      <title>Problem with AN3927 using JM60 in windows 10</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-AN3927-using-JM60-in-windows-10/m-p/1094499#M23190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;i'm trying to use AN3927 for a msd booloader on JM60, but, always there's a error message "Device cannot start(code 10)" in device manager. I'm using Wireshark to see the communication between host and device(JM60) and i saw a problem with "Get Max Lun Response". The device don't send the correct information and the problem i called happens, but, in windows Xp it works normally. what change in code i need to do for solve the max Lun packet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107315i847AB88DE92E54BD/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2020 18:33:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-AN3927-using-JM60-in-windows-10/m-p/1094499#M23190</guid>
      <dc:creator>eduardo1</dc:creator>
      <dc:date>2020-07-27T18:33:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with AN3927 using JM60 in windows 10</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-AN3927-using-JM60-in-windows-10/m-p/1094500#M23191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I solved the malformed packet problem with max get lun, but, i saw the scsi commands routines doesn't works. There isn't return with Inquiry command routine. How the microcontroller knows the variable who send the information to the host? I need to pointer to this variable and i don't know which is.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2020 12:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-AN3927-using-JM60-in-windows-10/m-p/1094500#M23191</guid>
      <dc:creator>eduardo1</dc:creator>
      <dc:date>2020-07-28T12:28:37Z</dc:date>
    </item>
  </channel>
</rss>