<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: P89LPC922 Security bits in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091929#M23181</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wrzuciłem wszystko tutaj :&amp;nbsp; &amp;nbsp;&lt;A class="link-titled" href="https://github.com/kociejsko/lpc922_erase_Nucleo" title="https://github.com/kociejsko/lpc922_erase_Nucleo"&gt;GitHub - kociejsko/lpc922_erase_Nucleo&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2020 13:14:40 GMT</pubDate>
    <dc:creator>rafal_obirek</dc:creator>
    <dc:date>2020-07-28T13:14:40Z</dc:date>
    <item>
      <title>P89LPC922 Security bits</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091924#M23176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I have microcontroller LPC922 and he has some sectors locked with security bits ( 0x07 ).&lt;/P&gt;&lt;P&gt;In the documentation is written ( as I understood ) that "global erase" shall clear these bits with 0x00&amp;nbsp; ( parallel programmer )&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.keil.com/dd/docs/datashts/philips/ps_900.pdf" title="http://www.keil.com/dd/docs/datashts/philips/ps_900.pdf"&gt;http://www.keil.com/dd/docs/datashts/philips/ps_900.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I bought a programmer TOP2013 and during ERASE I have observed with logic analyzer what is written to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I expected there was written 0x72 order to FMCON register and than is few reads from FMCON to check if programming was successor not.&amp;nbsp; This checking takes around 4ms&amp;nbsp; and status is always F0 what tells that chip is BUSY&amp;nbsp; ( probably erasing is in progress ). But programmer doesn't wait until the status is 0x70 and breaks VCC and return SUCCESS.&lt;/P&gt;&lt;P&gt;Later after reading security bits is still the same and nothing changes.&lt;/P&gt;&lt;P&gt;Writing 0x07 to other sectors which were 0x00 before works perfectly, but restoring it back by global erase not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And my question is now :&lt;/P&gt;&lt;P&gt;1. When security bits for given sector is already 0x07 is it possible to restore it back with 0x00 via global erase at all?&lt;/P&gt;&lt;P&gt;2. How long can take the execution of GLOBAL ERASE for this chip ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2020 22:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091924#M23176</guid>
      <dc:creator>rafal_obirek</dc:creator>
      <dc:date>2020-05-29T22:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: P89LPC922 Security bits</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091925#M23177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update from yesterday : &lt;/P&gt;&lt;P&gt;I tok Nucleo board and I have generated sequence to send "global erase".&amp;nbsp; Status was changed from BUSY to READY after around 7ms.&amp;nbsp;&amp;nbsp; Security bits were succesfully erased. That means it is a bug in programmer or programmer application&amp;nbsp; TopAll8. After erasing all my microcontrollers with Nucleo board, I was able to program bootloader using TOP2013 and then access to uC via ISP.&amp;nbsp; Everything works now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2020 20:51:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091925#M23177</guid>
      <dc:creator>rafal_obirek</dc:creator>
      <dc:date>2020-06-01T20:51:12Z</dc:date>
    </item>
    <item>
      <title>Re: P89LPC922 Security bits</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091926#M23178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Witam,czy mógłbyś udostępnić kod do Nucleo na global erase?&lt;/P&gt;&lt;P&gt;Pozdrawiam,&lt;/P&gt;&lt;P&gt;JacekG&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jul 2020 22:02:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091926#M23178</guid>
      <dc:creator>jacekgałuszczyń</dc:creator>
      <dc:date>2020-07-06T22:02:42Z</dc:date>
    </item>
    <item>
      <title>Re: P89LPC922 Security bits</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091927#M23179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hej.&lt;/P&gt;&lt;P&gt;Teraz jestem na urlopie do 28 lipca więc nie mam możliwości.&lt;/P&gt;&lt;P&gt;Ale jak wrócę to się podzielę. Wszystko chyba jest jako projekt w środowisku Cube.  Spakuję i wyślę całość.  Mogę dodatkowo dać bootloader do poprawnego działania isp.&lt;/P&gt;&lt;P&gt;Ustawiłem sobie przypomnienie na telefonie to nie zapomnę.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards/MfG/Pozdrawiam&lt;/P&gt;&lt;P&gt;Rafal Obirek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 03:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091927#M23179</guid>
      <dc:creator>rafal_obirek</dc:creator>
      <dc:date>2020-07-07T03:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: P89LPC922 Security bits</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091928#M23180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dzięki, miłego urlopu.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 07:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091928#M23180</guid>
      <dc:creator>jacekgałuszczyń</dc:creator>
      <dc:date>2020-07-07T07:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: P89LPC922 Security bits</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091929#M23181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wrzuciłem wszystko tutaj :&amp;nbsp; &amp;nbsp;&lt;A class="link-titled" href="https://github.com/kociejsko/lpc922_erase_Nucleo" title="https://github.com/kociejsko/lpc922_erase_Nucleo"&gt;GitHub - kociejsko/lpc922_erase_Nucleo&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2020 13:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/P89LPC922-Security-bits/m-p/1091929#M23181</guid>
      <dc:creator>rafal_obirek</dc:creator>
      <dc:date>2020-07-28T13:14:40Z</dc:date>
    </item>
  </channel>
</rss>