<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: what are the programming pins of P87C51MC2? which Programmer can i use ? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082924#M23154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mr.Vicente,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for answering my questions. I am working on the project in which the Old microcontroller is Obsolete (P89C51RD2BN): I just need to change the microcontroller to an available one. I am a hardware engineer and want to use an available microcontroller belonging to the same family so i change just the HW-Conception (with some small sw changes).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jul 2020 13:35:53 GMT</pubDate>
    <dc:creator>karim_ben-ali</dc:creator>
    <dc:date>2020-07-27T13:35:53Z</dc:date>
    <item>
      <title>what are the programming pins of P87C51MC2? which Programmer can i use ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082922#M23152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Guys,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the microcontroller P87C51MC2 of NXP, but i can't understand how to program it.&lt;/P&gt;&lt;P&gt;can anyone help me to know which pins are used for the programming and if there is any programmers available in the market ? and which sw-tool can i use to program it in C/C++ ?&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;K.Ben Ali&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 14:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082922#M23152</guid>
      <dc:creator>karim_ben-ali</dc:creator>
      <dc:date>2020-07-23T14:59:15Z</dc:date>
    </item>
    <item>
      <title>Re: what are the programming pins of P87C51MC2? which Programmer can i use ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082923#M23153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please be aware that the P87C51MC2 is a very old device that is still active but is the last one of the 80C51 devices.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are starting a project I recommend you move to a new product like the &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-architectures/8-bit-s08-mcus:HCS08"&gt;S08 family &lt;/A&gt;or the &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mcus/lpc800-cortex-m0-plus-:MC_71785"&gt;LPC800 &lt;/A&gt;family (32 bit)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question this device is compatible with any 80C51 programmer, unfortunately, we do not have any available now, you can check with a partner like PEmicro or Elnec.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I remember the programming is using the RST, EA, PSEN, Ale and the UART pins&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66947iDD3066380BE2A636/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you need more information for the new devices&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2020 22:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082923#M23153</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-07-24T22:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: what are the programming pins of P87C51MC2? which Programmer can i use ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082924#M23154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mr.Vicente,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for answering my questions. I am working on the project in which the Old microcontroller is Obsolete (P89C51RD2BN): I just need to change the microcontroller to an available one. I am a hardware engineer and want to use an available microcontroller belonging to the same family so i change just the HW-Conception (with some small sw changes).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2020 13:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-are-the-programming-pins-of-P87C51MC2-which-Programmer-can/m-p/1082924#M23154</guid>
      <dc:creator>karim_ben-ali</dc:creator>
      <dc:date>2020-07-27T13:35:53Z</dc:date>
    </item>
  </channel>
</rss>