<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Seeking info - Motorola SC44125P microcontroller</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079204#M23142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, I do not have data of this part.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2020 18:35:24 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2020-04-15T18:35:24Z</dc:date>
    <item>
      <title>Seeking info - Motorola SC44125P microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079203#M23141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm hoping someone can help me out with this vintage 1980s microcontroller - the Motorola SC44125P.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is clearly an OEM version of a 6800-class microprocessor (see attached picture for pinout; the highlighted pins are those that differ from a stock MC6800).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The information I am after specifically:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Confirmation of which MC6800 variant this chip is based on (6800 / 6801 / 6805 / 6809 etc.), so I can look up the correct opcode table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Presence and size of onboard ROM and method by which said ROM can be read out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/105689iE426DA60A8C166BB/image-size/large?v=v2&amp;amp;px=999" title="SC44125.png" alt="SC44125.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2020 05:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079203#M23141</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2020-04-09T05:15:57Z</dc:date>
    </item>
    <item>
      <title>Re: Seeking info - Motorola SC44125P microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079204#M23142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, I do not have data of this part.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 18:35:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079204#M23142</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-04-15T18:35:24Z</dc:date>
    </item>
    <item>
      <title>Re: Seeking info - Motorola SC44125P microcontroller</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079205#M23143</link>
      <description>&lt;P&gt;I asked on another forum and after&amp;nbsp;some discussion and examination of the accompanying EPROM code, it was determined that the code uses the 6801 instruction set.&lt;/P&gt;&lt;P&gt;There were no calls that would redirect to internal RAM or ROM, so these two sections are unused. One example of this part was 'decapped' and was revealed to have a 6800 die inside the chip.&lt;/P&gt;&lt;P&gt;So, the SC44125 is a customized 6800 with 6801 instruction set and hard-wired address / data pins.&lt;/P&gt;</description>
      <pubDate>Sat, 27 Mar 2021 18:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Seeking-info-Motorola-SC44125P-microcontroller/m-p/1079205#M23143</guid>
      <dc:creator>meterman1980</dc:creator>
      <dc:date>2021-03-27T18:50:05Z</dc:date>
    </item>
  </channel>
</rss>