<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: using multiple MC9S08JM60 to program several MC9S08 in parallel in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/using-multiple-MC9S08JM60-to-program-several-MC9S08-in-parallel/m-p/1070179#M23129</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can use one JM to program the S08 devices using the OSBDM&amp;nbsp; and you can download the firmware and the hardware from&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.pemicro.com/osbdm/" title="http://www.pemicro.com/osbdm/"&gt;PEmicro | Experts in Embedded tools for Flash Programming and Development&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I do not know if this can be used in parallel to program several device at the same time&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Aug 2020 17:33:03 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2020-08-28T17:33:03Z</dc:date>
    <item>
      <title>using multiple MC9S08JM60 to program several MC9S08 in parallel</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/using-multiple-MC9S08JM60-to-program-several-MC9S08-in-parallel/m-p/1070178#M23128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer plans to build is own programmer JIG for his production line, he plans to flash/program 10 units of MC9S08PA/PL devices&amp;nbsp;in parallel (same firmware).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please advise what is the best way to build such a JIG, could the customer use&amp;nbsp;multiple &lt;A href="https://community.nxp.com/t5/tag/MC9S08JM60/tg-p"&gt;#MC9S08JM60&lt;/A&gt; chipsets in order to build such a JIG.&lt;/P&gt;&lt;P&gt;Maybe he can use&amp;nbsp;one&amp;nbsp;&lt;SPAN&gt;MC9S08JM60&amp;nbsp;device to flash/program&amp;nbsp;several MC9S08x devices in parallel?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;waiting for your kind response, thanks in advance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Shai&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 20:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/using-multiple-MC9S08JM60-to-program-several-MC9S08-in-parallel/m-p/1070178#M23128</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2020-08-26T20:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: using multiple MC9S08JM60 to program several MC9S08 in parallel</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/using-multiple-MC9S08JM60-to-program-several-MC9S08-in-parallel/m-p/1070179#M23129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can use one JM to program the S08 devices using the OSBDM&amp;nbsp; and you can download the firmware and the hardware from&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.pemicro.com/osbdm/" title="http://www.pemicro.com/osbdm/"&gt;PEmicro | Experts in Embedded tools for Flash Programming and Development&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I do not know if this can be used in parallel to program several device at the same time&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Aug 2020 17:33:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/using-multiple-MC9S08JM60-to-program-several-MC9S08-in-parallel/m-p/1070179#M23129</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-08-28T17:33:03Z</dc:date>
    </item>
  </channel>
</rss>